Part Number: TMP117EVM Other Parts Discussed in Thread: TMP117 Hi experts,
This is FAE Skylar responsible for GREE. My customer wants to use TMP117 in the refrigerator project and want ±0.1°C accuracy on 0°C. They want to use the TMP117EVM for test but…
Part Number: EVM430-FR6043 Other Parts Discussed in Thread: TMP117EVM , Dear Team,
is there an easy way to hook up TMP117EVM with EVM430-FR6043?
I have seen that the booster pack has an I2C interface but the TMP117EVM comes as an USB stick.
Regards
And…
Part Number: TMP117EVM Other Parts Discussed in Thread: TMP117 , MSP430F5528 , ENERGIA We want to make a Windows app that reads temperatures from the TMP117EVM.
Is there a TMP117EVM programming guide?
Is there a software library for .NET with sensor_write…
Part Number: TMP117EVM Other Parts Discussed in Thread: USB2ANY Hello,
I have a TMP 117EVM and I want to use a dual sensor configuration. I have some sensors that are made at our company that are attached to a flex pcb. I've actually already asked this…
Part Number: TMP117EVM Other Parts Discussed in Thread: TMP117 , USB2ANY , Hello!
I have a TMP117 EVM and I want to connect it to two thermal sensors on flex PCB. I've broken off the tmp117 using the perforation, connected the USB and whats left of the evaluation…
Part Number: TMP117EVM Other Parts Discussed in Thread: USB2ANY
Hello TI experts,
My customer tests TMP117EVM now, they have one questions.
IN GUI, they set Register Auto Read Delay to 1s ;
and they got a log as below ;
as you see, to 53:51:2, it sampled…
Part Number: TMP117EVM Other Parts Discussed in Thread: TMP117 , The TMP117 operating temperature is specified as -55C to 150C.
What temperatures can the EVM board be used at? Do I need to break off the sensor tip and add an extension above/below a certain…
Part Number: TMP117EVM I am using the TMP117EVM module for a temperature measurement.
My software uses the USBview 2.0 (available as part of the Windows 10SDK) to check if the module is connected and to read the serial number.
Whenever the module is connected…
Part Number: TMP117EVM Other Parts Discussed in Thread: TMP117 , SYSCONFIG Hello,
I have a TMP117EVM, downloaded the GUI and installed it on my computer and is successfully logging the temperature. My intended application however is to log the temperature…