Part Number: TMP144EVM Other Parts Discussed in Thread: TMP144 , Hello
Can we add additional TMP144 ICs to the chain. If yes then are they readable in the GUI.
Also Can we export the temperature data from the GUI?
Thank you
Varun
Hi Chase,
We do not have source code for the TMP144. The TMP144EVM comes with USB2ANY firmware loaded into the MSP430F5528, and the control of the TMP114 is done through the GUI. You can see the GUI's source code in the file UARTPacketCodec.js by pressing…
Yes, it is standard UART. It is being generated at the PC and only passes through the MSP430F5528. In the TMP144EVM GUI, this happens in the file UARTPacketCodec.js which is located here: https://dev.ti.com/gallery/view/THSApps/TMP144EVM/ver/1.0.1/app/UARTPacketCodec…
Hi,
As mentioned, this is on a similar device the TMP144 which has 2 bytes for the temperature data. This device has the same protocol so the commands should work the same on the TMP104. My set up uses the TMP144EVM which has 4 devices on it so my response…
Hi Fakuno-san,
When performing Global Address Acquire, you should always supply an address of 0. This will be the address of the first device. The first two bytes will pass through the first device, and then the device will disconnect downstream devices…