Hi Anand,
I apologize for the delay here. I have learned that the SN 29500 standard for calculating FIT does not differentiate between package and die failures (unlike IEC 62380) since it is based on transistor count, technology, and package type. The FIT…
Part Number: TMP236 Hi Team,
Our customer will use multiple TMP236 analog temperature sensors a few centimeters away from the MCU thru cables and would like to know how to reinforced the circuit. I have checked some application notes but most of them are…
Part Number: TMP236-Q1 I am working with TMP236-Q1 parts on a prototype board. According to the datasheet, the typical Tc is 19.5mV. However, measuring the mV output directly on 3 different sensors on temps ranging from 10C to 50C, the coefficient works…
Part Number: TMP236 Hello,
I was thinking of using this part to sense toroidal transformer temperature.
It would be mounted on the outside of the transformer directly over the windings on a small PCB.
Do you think the strong magnetic field in this location…
Part Number: TMP236 Hi Sir,
We are using LTC2997HDCB now, could you help to recommend a pin to pin or similar function part to replace? Better to have stock/good supply.
Customer used L TC2997HDCB by placing it close to heat source (locally).
Thank you. …
Part Number: TMP236-Q1 Other Parts Discussed in Thread: TMP235-Q1 , TMP235 , TMP236 , LM35 , TMP61 , TMP63 , TMP64 Dear TI team,
there is some contradictory information in the datasheet regarding the operation range of the sensor.
In the heading of datasheet…
Part Number: TMP236 I'm using SOT32 TMP236 analog temperature sensor. I mounted it with long pins far from the PCB to avoid heating from other components on the board. So the sensor is now "floating" in the air.
The output voltage is around…
Part Number: TMP20 Other Parts Discussed in Thread: TMP236 Hi,
We use the TMP20 in a temperature control application which is set to 30 °C.
The temp error at 30 °C is between 0.8 % and 1 %.
The max deviation (error) around 30 °C is 0.004 °C.…
Part Number: TMP235 Other Parts Discussed in Thread: TMP236 My customer HEMAI is using out TMP235 and syslink's CT7035 for P2P. And they are cusrious about the sensor gain parameter in the datasheet .
So what performance the sensor gain of a temperature…
Hi Ala,
Thank you for sharing these details. Since your main concerns are maximizing accuracy while using an integrated ADC I would recommend looking at TMP236-Q1 . This analog temperature sensor offers a max temp accuracy of ±2.5 °C accross the full range…