Part Number: TMP275 Dears,
Customer feedback that the TMP275 screen is different with the sample that they buy through TI Store before,pls help to check it.
Thanks
Part Number: TMP275 Hello TI Team,
We am planning to use TMP275 for temperature sensor and indicate the overheat in my PCB Board.
As we understood ALERT pin can be used as below,
We will set the T HIGH =40Deg and T LOW =38Deg.
When the temperature cross…
Part Number: TMP275 Hi, Support Team
About TMP275AIDGKR ,what is the SDA rise time value?
There is no TrD value in spec,please help to confirm.
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: TMP275-Q1 Other Parts Discussed in Thread: TMP275
Is it possible for the device to be in shut-down mode initially and then triggered to do a One-Shot conversion? What are the ramifications of triggering a one-shot conversion by setting the…
Part Number: TMP275 Other Parts Discussed in Thread: TPS82130 We have a few TMP275 sensors spread around in a system, connected by wires, and powered by a 5v TPS82130 (powering also some other relatively light loads).
What should be the 5v PS specifications…
Part Number: TMP275 Other Parts Discussed in Thread: TMP114 I am planning on using the TMP275 for on board temp sensing. It runs off 3.3V, but looking at the digital logic threshold, it's not possible to interface with 1.5V LVCMOS logic. Is there a solution…
Part Number: TMP275 Hi Team,
I aksed TMP275 I2C quetion in below e2e but I have additional question so could you hlep?
[Question 1] TMP275 reqires conversion time for conversion result. if we READ before finishing conversion time, what is the output data…
Part Number: TMP275 I need a temperature sensor recommendation with the following key specification:
3.3V Powered
I2C Interface with at least four addresses
-10 to 85°C range (min)
Isolated from ground sensing.
The last requirement is important and…