Part Number: TMP302 Hello,
We're working with the TMP302 and seeing some differences when device trips.
Which pin on the IC is being monitored for temperature?
Does is matter the level of solder used? Or how far off the PCB the IC might be?
Has there…
Part Number: TMP302-Q1 Hello Experts, My customer would like to know where the temp sensor is located in the chip. Would you tell it, please? Best Regards, Fujiwara
Part Number: TMP302 Hello,
We're using the TMP302 in an application and getting varying accuracy results.
Looking for some layout suggestions.
Which pin on the IC is used for temperature measurements?
Not able to connect up any pins on the IC to…
Part Number: TMP302 Hi, the trip point accuracy for TMP302 is shown as +-0.2C typical, +-2C maximum.
+-0.2C would be brilliant for my application, but +-2C is not good. Can you provide any information about the difference between typical and maximum trip…
Part Number: TMP302 Hi,
May I know if we have analysis done on TMP302 with conformal coating? Do we have any concern on the accuracy impact after conformal coating?
Thanks,
Christina
Part Number: TMP302-Q1 Hello,
According to TMP302-Q1 datasheet, if HYSTSET pin connect to GND, THRESHOLD HYSTERESIS is 5°C, if connect to Vs, it's 10°C.
What is THRESHOLD HYSTERESIS if HYSTSET pin left floating?
What kind of symptom is occurred…