Part Number: TMP411 Hi Team,
My customer is not using the remote sensor function, so they follow the DS description to short the D+ and D- together as below.
There is a question about the Pin6 behavior. Before any configuration or setting. The customer…
Part Number: TMP411 Hi Team,
I want to follow up the further question of the E2E post below.
(+) TMP411: not using remote sensor - Sensors forum - Sensors - TI E2E support forums
Since the customer is not using the remote temp function, they…
Part Number: TMP411-Q1 Hi team,
Whether we have device could measure -100℃? Customer would like to test liquid nitrogen temp, it is very lower.. Whether we could have device to support?
Part Number: TMP411 Hello,
I want to measure the temperature of some mosfets mounted on a heat sink as accurate as possible. I would send the Temperature to MCU, my Question ist:
If I used the Tmp411 with pnp Transistor, I want to connect the ground…
Part Number: TMP411 we are looking to use this device for measuring temperature from an on chip Thermal Diode. The device can be supplied using 3.3V but for the I2C interface - we need to pull the SCL, SDA lines to 2.5V not 2.7V as recommended. Can this…
Part Number: TMP411 In the file: TMP411 SBOS383D –DECEMBER 2006–REVISED DECEMBER 2016 page 12 below is mentioned that it is possible to measure temperature up to 191 °C. Can you confirm that it is correct?
Can you please help me with the external sensor…
Part Number: TMP411 Other Parts Discussed in Thread: TMP451 , TMP461 , TMP1075 , TMP235 Hi sir,
I am planning to use the TMP411 temperature sensor for my design to measure the temperature of a clock synthesizer.
Since the clock IC doesnt have dedicated…
Part Number: TMP411 Dear Team,
The customer use TMP411 to replace ADM1032.(The ADM1032 work fine here)
But the remote temperature can’t be read, and it shows around 0 degree C at room temperature.
Could you help to check is there anything we need…