Part Number: TMS320C5535 Hello I am New to Code composer studio i have worked on TMS320C5535 ezdsp kit but dont have any software related sources like as CD drive and Memory card.
I have found this user guide ( http://www.ti.com/lit/ug/tidubj5a/tidubj5a…
Part Number: TMS320C5535 Hi
fatal error #16004: file "D:/TI-DSP/Software Downloads/C5535-eZdsp-master (1)/C5535-eZdsp-master/lib/ezdsp5535bsl.lib<ezdsp5535_lcd.obj>" has a Tag_Memory_Model attribute value of "2" that is different than one previously…
Part Number: TMS320C5535 Other Parts Discussed in Thread: BOOST5545ULP , CCSTUDIO , SYSCONFIG Hi,
From TI we are purchased TMS320C5545 based BOOST5545ULP EVK for one of our FFT development using HWAFFT. So, is it possible to provide some sample source C…
Part Number: TMS320C5535 Hi
i am new beginner to TMS320C5535 ezdsp
im using aic3204 on a ezDSP C5535 based design board,in the event of trying to capture audio from open source codec
#include "stdio.h" #include "ezdsp5535.h" #include…
Part Number: TMS320C5535TMS320C5535 question
1. does IC external flash ?
2. How much does flash support?
3. IC / flash interface
4. programming language ?
5. First time factory burning CODE method? (USB? JTEG?)
Part Number: TMS320C5535
Hello,
We are planning to implement time critical 512-point FFT algorithm using any one of TI "HWAFFT" supporting processor.
Please suggest mostly available TMS320 series part number in the market with best performance…
Part Number: TMS320C5535 Can C5535 CLKIN support other frequency other than stated in datasheet?
Such as 18.432MHz, 19.2MHz, why if not ? what will impact?
Part Number: TMS320C5535 I tried a simple test and the behavior of the PERI_TXCSR register does not seem to follow the spec.
I'm using address 0x8512 for non-indexed version of endpoint 1 register.
TXMAXP is set to 800 and the FIFO is configured for…
Part Number: TMS320C5535 If build project with -vcore:2.2, can it run on a V3.3 C55x device.
Is there a list of difference between V2.2 and V3.3 C55x CPU?