Hello Paul ,
Thank you for your reply.
PaulM said: Does CLKOUT1 exhibit the same behavior?
When is reset released (in relation to CLKOUT2 becoming stable)?
The datasheet shows that CLKOUT2 is undefined until 20ns (based on 200MHz CPU clock) after reset release…
Part Number: TMS320C6204 Hi, I have a question from customer who uses C6204. Does the PLL inside the device have different characteristics under different temperature? If so, how temperature change affects to PLL output including CLKOUT? Or As far as temperature…
Part Number: TMS320C6204 Dear TI I would like to know the ESD (MM/HBM/CDM) rating of TMS320C6204.
A customer of mine is asking for the ESD ratings so that they can protect against harming the part during handling and loading on PCB. Please advise.
Best…
Part Number: TMS320C6204 Dear TI I would like to know the ESD (MM/HBM/CDM) rating of TMS320C6204.
A customer of mine is asking for the ESD ratings so that they can protect against harming the part during handling and loading on PCB. Please advise.
Best…
Part Number: TMS320C6204 Hello,
Regarding to land pattern example on TMS320C6204 series(below) ,my customer is asking a question.
TMS320C6204ZHK200
TMS320C6204ZHKA200
(Question)
Do you have land pattern/solder paste example of MicroStar BGA on above…
Other Parts Discussed in Thread: TMS320C6204 My customer is going to input the spread spectrum clock into CLKIN of TMS320C6204.
This is because ASIC which he use with the same clock carries out necessity of the spread spectrum clock.
A spread spectrum…
Other Parts Discussed in Thread: TMS320C6204 I'm new to this whole world and want to connect an XDS-560v2 to a TMS320C6204 DSP device via JTAG but I don't see the option in Code Composer. I've seen this guide:
http://processors.wiki.ti.com…
Other Parts Discussed in Thread: CCSTUDIO I have been trying for the last week to install CCS 5.2 onto a new computer with no luck. It appears some of the features install but not all. I require assistance to the problem. Below is the log.
[ Edited by…