The actual solution of the "howto flash external flash ROM via EMIFA" problem is still missing in this forum article. I will add a short summary of how i got a working solution. 1. We dropped restoration of WindowsXP 2. We dropped using CCS3.3 …
Part Number: TMS320C6455 Other Parts Discussed in Thread: CCSTUDIO , I'm trying to do some configuration management on some DSP devices I have (using a 6455 DSP). I want to either fully read back the firmware, or at least get a checksum so that I can track…
Part Number: TMS320C6455 My customer is looking to add the TMS320C6455BCTZ2, which is a 1.2GHz part as a substitute for TMS320C6455BCTZ. It appears that the 1.2G part should be a drop in replacement for the 1G part, without a need to change on-board clocks…
Part Number: TMS320C6455 Hi Team,
Is the L2 SRAM of C6455 only used for SRIO? I notice that C6455 allocates memory space for PCI but does not allocate memory space for SRIO. I s the peripheral access to SRIO local memory equivalent to accessing the L2…
Part Number: TMS320C6455 Hi,
I have a FPGA and DSP in my custom designed board,
FPGA and DSP are communicated over EMIF interface and GPIO5 is connected between DSP and FPGA.
FPGA sends the interrupt to DSP before data transfer.
But I am getting the error…
Part Number: TMS320C6455 What are the thermal reflow differences between TMS320C6455DCTZA8 and TMS320C6455DZTZA8 for soldering purposes? Both devices seem identical in the datasheet with the difference being in the Pb-free solder balls and die bump.
Part Number: TMS320C6455 For TMS320C6455 want to bypass the HAL layer and want to do the configuration below,
Specifically, the following configuration is desired.
CPU core PLL set to 750MHz from a 60MHz oscillator.
Timer0 set to increment on a 100uS…
Part Number: TMS320C6455 Hi, My customer wants to make sure the workaround for Advisory 3.1.21 is valid in their system. https://www.ti.com/lit/er/sprz234r/sprz234r.pdf Under which conditions (voltage, temperature, etc.), the issue likely occurs? They wants…
Part Number: TMS320C6455 the PCI_EEAI pin has been enabled to auto load PCI registers from EEPROM. We want to confirm if there is some reliability issue if we change the 0x403 (revision_ID) from 0x1 to 0x2. I assume there should be ok to do such change…