Part Number: TMS320C6711D So far I have the following errors when compiling using CCSV7.0
**** Build of configuration Debug for project scenepro-ins ****
"C:\\ti\\ccsv7\\utils\\bin\\gmake" -k -j 12 all -O gmake[1]: Entering directory 'C:/Users…
Part Number: TMS320C6711D Dear TI support team,
I am submitting this help request as the problem we are facing with TMS320C6711D is similar to the one reported in the Thread "TMS320C6711D: DSP not responsive after a period of inactivity". We have…
Part Number: TMS320C6711D Dear TI support team:
Im am doing some final testing on equipment that uses TI DSP and suddenly the DSP stopped working (after leaving it alone for about 1 month in a clean room environment it is no longer responsive)
Nominally…
Part Number: TMS320C6711D We are replacing the obsolete TMS320C6711BGNA100 with the TMS320C6711DGDPA167. Should we expect much of a change in the output drivers (strength, edge rate, etc) or are they very similar? I'm specifically looking at the address…
Part Number: TMS320C6711D Hello,
We are using the C6711D in our product and we meet a rate of 20 to 40% of unsuccesfull starts.
Our software boot in internal flash on a boot loader witch load the firmware in RAM. The first instruction of our boot is to…
Part Number: TMS320C6711D void PLL_Configuration()
{
int i; //JFV 30/11/2006 here for the wait loops
//PLLCSR &= 0xFFFFFFFE; // set PLLEN to 0
PLLCSR = 0x40; // set PLLEN to 0
for (i=0; i<5; i++)
{} // wait for 4 CLKIN cycles
//PLLCSR…
Part Number: TMS320C6711D Hello Guys,
Good day.
Our customer wants to know if it is possible to set a "watchpoint" with the XDS560v2 on the tms320c6711D? They want to know if this processor has the internal function to set a "watchpoint" (hard breakpoint…
Part Number: TMS320C6711D Hi TI team,
Good day!
We have a customer's inquiry regarding the installation guide for or TMS320C6711 IMAGING DEVELOPERS KIT SOFTWARE v1.10.
Is there any available installation guide for this device?
Thank you in advance for…
Part Number: TMS320C6711D Tool/software: Code Composer Studio I'm using CCS 10.1.1.00004 and a Blackhawk XDS560v2 emulator. To debug this I've created the 'Hello world' example application. If I run Test Connection in the target configuration window I…
Part Number: TMS320C6711D
Hello,
I am trying to design a test bed for digital beamforming using constant modulus algorithm. Before going to hardware, I wanted to simulate a virtual test bed design in simulink using TI DSK processors in SIMULINK (MATLAB…