Part Number: TMS320C6713B I am going to convert my old project CCSV3 to CCSV5 using the new project method but my main code include TSK_sleep(1); But this function comes from old bios tsk.h. So I can't match it with the new bios. How do I include tsk…
Jay
these are always a challenge to find root cause. Best I can offer here are some things to consider.
- Possible power issue that only occurs under a specific set of conditions. Could be external (surge/brownout), could be a weakness in the PDN to supply…
Part Number: TMS320C6713B
https://software-dl.ti.com/ccs/esd/documents/sdto_cgt_Linker-Command-File-Primer.html
The "Additions and Changes" part in above link suggests readers to post code of linker command file which is not described in that…
Part Number: TMS320C6713B Dear Sir or Madam,
When using this device, "TRST" is Open, "RESET" is energized at High level (normal operation setting)
You may have unintentionally set "EMU1" and "EMU0" to Low (set to Boundary Scan) at…
Part Number: TMS320C6713B Hello,
TMS32C6713BGDPA200 DSP is used as DSP in some of the cards. This DSP stores boot code and some of the system parameters on EMIF flash (INTEL TE28F320C3TD90). Some of erroreneous DSP cards, at the start up (boot), some…
Part Number: TMS320C6713B Hello,
I recently tested the DSK6713 development board, the development environment is CCS5.5, and then the computer environment is win10 home Edition. The emulator uses an onboard USB emulator, and the problem is that it keeps…
Part Number: TMS320C6713B Hi experts,
My customer is using TMS320C6713B.
they are reviewing in C6000's complier defects. however, the like to the detail DOC of each ID is not opened.
I'd like to check the detail of the items below.
CODEGEN-14…
Part Number: TMS320C6713B I'm using CCS v5.3 to compiler and run code on simulator for TMS320C671B target configuration. I could able to code and run my program. Now I want to do CPU profiling on Simulator. Is there a way to do that. I mean how to measure…
Part Number: TMS320C6713B hello?
We are constructing the circuit diagram of the TMS320C6713B product.
While reviewing the catalog, EMI FILTER is used in the recommended circuit. However, ACF451832 and EXCCET103U products are discontinued.
I am inquiring…
Gary
I could not locate the document you referenced - Application of TI C64x+DSP Kernel Exception Handling Mechanism.
The only document I found that may have relevant information is https://www.ti.com/lit/pdf/spru733?keyMatch=SPRU733A
--Paul