Part Number: TMS320C6747 Hello Team,
TMS320C6747 are there any more detailed power-on timing requirements, the specific time required for power-on timing, or the schematic diagram of power-on timing?
Thanks!
Part Number: TMS320C6747 I am trying to port a function from GCC to the TI compiler v7.4.4 for the C6000. In GCC, here is an example function. It include a per function optimization option:
__attribute__ ((optimize("-O3"))) uint32_t _unpack_bin…
Part Number: TMS320C6747 Looking for "real_fft_demo_c674x.zip" which is a file referred to in spracn4, Using DSPLIB FFT Implementation for Real Input and Without Data Scaling.
The link in the doc is dead. I would like to see the contents.
Part Number: TMS320C6747 Other Parts Discussed in Thread: TMS320C6745 , OMAP-L137 , I'm using a C6747, and trying to QDMA a small block of data from an external FPGA into local RAM - essentially a background memcpy() type operation, and ideally without using…
Part Number: TMS320C6747 Hello,
I have just migrated from CCS v5.2.0 to v9.1.0 and it seemed to go very smooth. I created my *.out file with no errors or warnings. For v5.2.0, we used AISgen for D800K005. Do I still use this for the *.out for v9.1.0?…
Part Number: TMS320C6747 Hi TI,
I have use TMS320C6747DZKB3 (375M) to develop my previous project, both CVDD and RVDD are 1.2V.
Now, I use TMS320C6747DZKB4 (only work in 250M) to develop my new project. I want know whether I could use previous power solution…
Part Number: TMS320C6747 Sir/Madam,
I am using Code Composer Studio V12 to try to write a program for the DSP using mcasp. To this end, I am using the quick start CSL examples. However, I got stuck trying to add an include path. How do you add an include…
Part Number: TMS320C6747 Sir/madam,
I am using Codec AIC3106 and ADC6140 interfaced DSP TMS320C6747 via McAsp1 and McAsp0 ports.
Codec or ADC samples are read/written using EDMA peripheral. EDMA will generate interrupt after collecting/sending one frame…
Part Number: TMS320C6747 Sir/Madam,
I tried to compile McASPEcho for TMS320C6747 but I got the error "rts6840.lib not found". I searched my drive and found rts6740_elf.lib and rts6740e_elf.lib only. What should I do now? Help much appreciated. Thanks…
Part Number: TMS320C6747 Sir/Madam,
I have installed aer_c64Px_obj_17_0_0_0_Win32 but when I try to compile, I got a build generation error asking for ti.mas.aer.c64Px. What should I do now?
Many Thanks in advance.
CCPoon