Part Number: TMS320C6748 Hi,
Good day,
I am using TMS320C6748 module. I am creating the Bootloader using AISgen tool.
Bootloader is working fine. but without any reason, boot loader is corrupted, and it needs to be Flash the boot loader once again.
it is…
After the file header and the data set header, the .pdat file should be a copy of memory starting at the address marked by the symbol __TI_prof_data_start . Have you compared the contents of the .pdat file with the contents of memory at that address? Do…
Part Number: TMS320C6748
Hi There,
We have a custom board we are bringing up. It's based on the C6748LCDK. We're using the PDK in a baremetal way.
I'm working to toggle the GPIO pins, but I'm having trouble: After modifying the board_cfg.h file…
Part Number: TMS320C6748
Hello. I have some trouble about float-point.I have this code: double a = pow(10, -320);
double b = pow(10, -20);
printf("a is %e", a);
printf("b is %e", b); The console is : a is 0.000000e+000 b is 1.000000e…
Hello Cayden
Thank you.
If i am understanding correctly the board has not issues when powered up or during repeated power-ups.
The issue seen is with the manual reset.
Have you removed the cap at the output of and gate.
Can you please measure the AND gate…
Part Number: TMS320C6748 I'm trying to automate the firmware build for a TMS320C6748 and I'm running into a problem making use of AISGen inside of a docker container as part of a CI build pipeline. In my office, we can only use Linux based docker…
Part Number: TMS320C6748 Other Parts Discussed in Thread: MATHLIB Is there any intrinsic support for C6748 DSP or do we have to go with assembly coding? We are referring TMS320C6748 DSP Technical Reference Manual but it has only Assembly OPCODE instructions…
Part Number: TMS320C6748 I am using code composer studio v5.3 which is supporting simulation for TMS320C6748 and I want to Profile my code to know which part of code is taking how much cpu. I haven't found any resources to do that. give any example code…