Part Number: TMS320DM365 Hi
I would like to get any information about DM365.
Q1. Is there anything information about DM365 FD register and FD detail?
Q2. If Replace DM365ZCED to DM365 that have FD, Is there any probrem occord by that unusing FD and software…
Part Number: TMS320DM365 I wanted to know more this chip. I am working on a circuit that was built in the late 90's and within that chip they used to produce an analog video signal using a video sync separator/stripper, that would feed into an ADC from…
Part Number: TMS320DM365 Hello, we are searching for solution to make such a camera: 1. First stage - we use external camera with YUV4:2:2 output at the moment. We need upscale image (from YUV4:2:2) 2-3 times and output it to the YUV4:2:2 or 24bits…
Part Number: TMS320DM365 Hi,
I'm using DM365 to drive an oled which takes 720P 8 bit ycbcr video with embedded sync.
I'm using RDK V5.10 and ipnc_psp 3.21.0.4 version. I have made changes to give output clock to 74.25 M hz and on probing the pixel…
Part Number: TMS320DM365 Tool/software: Code Composer Studio Hi,
I was using CCS V3.3 + XDS510USB to work with my DM365.
Now I want to transfer to a higher version CCS because if Win 10 system is used.
But when I tried to use CCS V9.3, I always get a…
Part Number: TMS320DM365 We would like to change NAND flash.
Could you check if TMS320DM365 can suppoort the following new NAND flash and the software compativility between current one?
[Current NAND flash]
Vendor: Hynix
Part Number : HY27S1G8F2CFR-BI …
Part Number: TMS320DM365 In the DM365 processor there is a sd card recording feature , using " Appro_avi_save " which is implemented using armffmpeg.
My query is that, how does the recording feature work.
How the data flows from the DM365 to …
Part Number: TMS320DM365 I was contacted by a customer who is working on an update to a DM365 application. He accidentally erased uboot from the Flash on the board and was wondering if he can the Uboot binary and flashing tool to fix the issue.
Thanks…
Part Number: TMS320DM365 Tool/software: Linux Hello,
Could you tell me the configurations to build the ALSA Library (ver1.1.6) in DVSDK for TMS320DM365? My customers tried to re-install the ALSA Library; however, the output file is four times larger than…