Part Number: TMS320F2800157-Q1 Tool/software: Hi,
I need the STL library for the TMS320F2800157-Q1 microcontroller. Where can I request access to that resource?
Best Regards Andreas Brenner
Part Number: TMS320F2800157-Q1 Tool/software: Hi Team
we have a requirement on sensisng the position of the flight control surface, And we have selected F280037CPTQ1 for the application.
I would reqest you team to letus know the EOL(longevity) and…
Part Number: TMS320F2800157-Q1 Other Parts Discussed in Thread: C2000WARE Tool/software: I have a question during the development process.
While performing power ON/OFF testing, I encountered an intermittent issue where LIN communication fails to operate…
Part Number: TMS320F2800157-Q1 Tool/software: we converted 4 wire to 2 wire JTEG and also reduced the TCK frequency also wrapped the wires, but still i am facing the JTEG disconnection issue.
Part Number: TMS320F2800157-Q1 Tool/software: Hi experts,
my customer asked if we have Voh vs Ioh line, and Vol vs Iol line.
Now they are checking the useable devices to connect with 2800157 GPIO to avoid risk. The Ioh is about 3mA. They want…
Hi,
I can't understand what the question is here.
Why can't you power-on chip and flash program, why is MCU reset is required ?
Reed said: After powering on, manually lower the reset signal DSP-REET once or pull the reset chip CT signal to 3.3V…
Part Number: TMS320F2800157-Q1 Tool/software: I am using a TMS320F2800157EVM launch pad to connect to a TMS320F2800157-Q1 on a motor controller. JTEG is getting disconnect when I go to higher supply voltages from 24V to 48V.
Up to 30V it's working fine…
Part Number: TMS320F2800157-Q1 Other Parts Discussed in Thread: MIDAS Tool/software: Hi team,
I ask this for my customer.
In their application, they don't use external WD, but in Midas, this is not be modified and always be enabled
How can they…
Part Number: TMS320F2800157-Q1 Tool/software: Hi team
My customer is using the flash_kernel_ex3_sci_flash_kernel to receive the new firmware through SCI and program it to flash.
They refer the user guide: Serial Flash Programming of C2000 Microcontrollers…
Part Number: TMS320F2800157-Q1 Tool/software: Hi experts,
My client is evaluating 2800157-Q1.
They want to know if VDDIO and VDDA drop from 3.3V to 3.2V, will the internal reference (2.5V & 1.65V) have a voltage drop?
Thanks,
Leo