Hi Yoel,
It seems like you are looking for something similar to the SCI Example for Echoback or SCI Flash Kernel for the F28004x device (which takes some basis from the bootROM code for SCI, and has a Flash build for loading the code). These projects…
Part Number: TMS320F280045 Other Parts Discussed in Thread: C2000WARE
Hello, I would like to configure my ADCA A2 for oversampling. As shown in the concept diagram, in the picture below.
I would like to use EPWM1 as 16kHz PWM, and with that I would like…
Part Number: TMS320F280045 I use INTOSC1 as DCCCLKSRC0 and SYSCLK as DCCCLKSRC1, This means comparing the frequency error between INTOSC1 and SYSCLK. Recently,a device display a DCC error, so I carefully studied the use of DCC. My understanding of this…
Part Number: TMS320F280045 Hi.
I'm using the XDS110 DEBUG prob. on our card which contains the 280045.
the Debugger works fin. but when I try to correct the code and run a debug session, I receive the following ERROR.
Error connecting to the target…
Part Number: TMS320F280045 I'm using the 280045 ADCs
I'm trying to use the internal 2.5V vref but I get result from the ADC which are corresponding to the\external 3.3V.
this is the code I'm using:
// Enable the temperature sensor output to…
Part Number: TMS320F280045
Hi.
I'm running a code on the F280045.
I'm using the XDS110 DEBUG PROBE.
Usually when I run a code that is mapped to the FLASH, the code is FLASHED into the device, and after I disconnect from the Debugger and power…
Part Number: TMS320F280045 We are getting closer to the root problem. We found out that it was an NMI (more specifically an NMI of the PLL) that was causing this strange behavior from our last post (TMS320F280045: Incorrect ISR jump address) .
Apparently…
Part Number: TMS320F280045 Dear All,
I am using the GPIO8_x2 as an LED . According to data sheet ,it uses INTOSC2 for configuration but even by proceeding that way still its not working in continuous run , but if I use breakpoints on the LED then it glows…
Part Number: TMS320F280049
Hi Champs,
If the voltage on the comparator positive input is greater than the voltage on the negative input, it will set comparator output to 1 and set CTRIPH/L to trigger EPWM protection. This is the way we are used to.
I want…
Part Number: TMS320F280045 Other Parts Discussed in Thread: SYSCONFIG , C2000WARE Is there a way to create a blank TMS320F280045PM (64 pin LFQP) SysConfig project in the Code Composer Studio (CCS) without starting from an example project?
I found this: …