Part Number: TMS320F280048-Q1 Other Parts Discussed in Thread: C2000WARE Hello Experts,
For those flash programming, I one used code from example " flashapi_ex1_program_autoecc.c" from C2000Ware . There is one function (Fapi_doVerify)applied as…
Part Number: TMS320F280048-Q1 Dear TI Team,
Getting from the Mahindra & Mahindra, we are facing the problem on MCU " F280048PMQR" from one of our OBC (on board charger) supplier, For Vehicle on board charging application.
The particular MCU…
Gokhan G. said: 1) Can I program and use PWM5 or 6 or 7 in order to generate predefined intervals(every 1.25us) for ADC soc trigger without any misfunction on SPI and UART?
Yes, we do not need to bring the PWM to a physical GPIO pin, we just need to use…
Hi Gokhan,
The PWM registers will instantaneously update as you execute that particular instruction. Can you please put a breakpoint just before exiting the ISR and check what all registers have not been updated WITHOUT the delay being added?
Can you…
Part Number: TMS320F280048-Q1 Other Parts Discussed in Thread: C2000WARE Hi experts,
Do have static codes test on the C2000Ware driverlib and corresponding reports? Customer used driverlib in their project, and requests for the static codes test report…
Gokhan G. said: I cannot trip my EPWM2. Gus says that if any ePWM is progrramed as CBC, it cannot be OST. My ePWM2 is CBC and I cannot trip it using OST. If it is impossible to trip using OST, I need to know it. Then OK.
There is only one trip-zone module…
Part Number: TMS320F280048-Q1 Hi,
I saw some kind of usage of __attribute__(()) in some reference software. I'm trying to understand what they are and what their help is.
1) What does it to do writing __attribute__((ramfunc)) on the line before writing…
Part Number: TMS320F280048-Q1 Hi,
After implementing DCL to my current working software on flash, it is required to reload the program to flash after re-energising my board. That means I always need to re-load program to flash again, after powering off…
Gokhan G. said: Q1) May the test condition wrong to test CMPSS? I use CR of electronic load and it is 0.25ohm. However, the output voltage varies depending on the current inside of CMPSS. That changes output voltage and duty.? Should I change the test…
Part Number: TMS320F280048-Q1 Other Parts Discussed in Thread: SYSCONFIG Hi,
I have driverlib based project. I separately test the below trip functions which works fine.
Now, I want to use combination of all as below. I wrote below lines but it didn't…