Part Number: TMS320F280049M Other Parts Discussed in Thread: TMS320F280049 Tool/software: TI C/C++ Compiler Hi Team,
My customer reported an warning while using TMS320F280049 CLA for using HRPWM: Using "#Define" to define a variable in constant address…
Hi Marlyn,
I tried following the guidance from this question: https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/676803/tms320f280049-serial-flash-programming-issues
However, I'm not 100…
Hi Jejomar,
Jejomar Ildefonso said: 5. SFO lib Driverlib implementation in EABI format - SFO_v8_fpu_lib_build_c28_driverlib_eabi.lib 6. Index lib for Driverlib based SFO lib - SFO_v8_fpu_lib_build_c28_driverlib.lib
Number 6 is the index library for…
Siddharth Deshpande said: Was C2000Ware installed from Resource Explorer or did you download and install it from ti.com?
Looks like Corey downloaded from ti.com and manually installed it since the C2000Ware is installed in C:\ti\c2000. That is the default…
Unknown said: I can allocate ca. 2x less than available.
The confusion is that the CCS Memory Allocation view displays the memory usage in terms of 16-bit words, but labels the values as "x out of y bytes used". Where "bytes" is normally taken to be…
Hello David,
Yes, most of the C2000 device families have QEP peripherals integrated. Some options would be:
F28007x: 120MHz, up to 3 eQEP: https://www.ti.com/product/TMS320F28075
F28004x: 100MHz, up to 2 eQEP: https://www.ti.com/product/TMS320F280049…
Hi, Can you refer this post and let me know if it helps? https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/838289?TMS320F280049-Active-high-complementary-PWMs This seems to refer to the same issue you've explained here, if i understand correctly…
Vivek,
and I also checked the method you metioned in this thread:
https://e2e.ti.com/support/microcontrollers/c2000/f/c2000-microcontrollers-forum/905675/tms320f280049-failed-to-verify-image-after-load-image-using-uniflash-if-dcsm-is-configured
…
Part Number: TMS320F280049C Other Parts Discussed in Thread: C2000WARE Tool/software: Hello,
I am using the TMS320F280049C MCU and want the device to implement LDFU through SCI. I have been reading related documentation: sprabv4, tiduey4d, spruiu8a…
Hi,
I think it is because PowerSUITE is not automatically installed. Please refer to the thread below and let me know if this helps. Thanks.
http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/864602?TMS320F280049-import-CCS
Regards,…