Other Parts Discussed in Thread: TMS320F28016 Dear all, we realized some prototypes of a sensor with TMS320F28016 DSP
for our customer.
We needed a fast setup for programming the flash through jtag interface and we intended to use a
ELPROTRONIC Flashpro2000…
Hello,
I have a very simple problem, I could not solve unfortunatly. I need to measure the loop time of my application. With other controllers I would simply start a timer at the beginning of the loop, save its count to any variable and reset the timer…
Hi All,
We build 2 project likes an OPT(User boot code) and flash(User application code) memory and we made each *.out file.
In the case we need two programming to OTP and Flash memory using the JTAG or bootloader.
Let me know how can merge each *.out…
Nicolas,
It would be best to contact The MathWorks. I suspect that the issue is that the linker command file used by Simulink doesn't match with the memory layout of the TMS320F28016.
Here is the memory map from the data sheet for the device:
The…
I got one more understanding issue : In the datasheet it says:
"The
TMS320F2809 ,TMS320F2808,TMS320F2806,TMS320F2802,TMS320F2801,TMS320F28015
,TMS320F28016,TMS320C2802,and TMS320C2801 devices,members of the
TMS320C28 x™ DSP generation,are highly…
Other Parts Discussed in Thread: TMS320F28016 Hi everyone,
I'm working with an old board used for motor control. This board places a TMS320F28016PZA, with 32Kb for flash memory. Right now I'm near to complete the flash capacity, so I would like to replace…
Oh, damn, my bad. I finally found it. The right option to choose is:
"Connection" > "Texas Instruments XDS100v3 USB Emulator" (in CCS v5.5)
i got one more question: I also use the development board, Olimex TMS320-P28016....it…
Other Parts Discussed in Thread: TMS320F28016 Hello everyone,
I’m using the TMS320F28016 DSP and CCS3.3 compiler. My programme is near to finish, but I have a few loose ends. For example, I would like to save the software version into the .out file .…
Other Parts Discussed in Thread: TMS320F28016 Hi all,
I am working right now with a DPS model TMS320F28016, to control it I am using an FOC engine. This system consists on moving a piece from an initial position to a final position (initial and final position…
Other Parts Discussed in Thread: TMS320F28016 Hello,
I’m being implementing a FOC controller for a PMSM motor, using a TMS320F28016 with a 256 pulses encoder. I’m close to the end of my project, but right now I have some problems. Specifically, when the…