Other Parts Discussed in Thread: TMS320F28016 Hello everyone,
I'm working with the TMS320F28016 DSP and CCS3.3V. I've implemented a wathdog function in my code, and right now I'm trying to test this function.
In order to do that, I execute…
Other Parts Discussed in Thread: TMS320F28016 Hello,
I'm working with CCS v3.3, a Blackhawk emulator (USB 2000) and a board with a TMS320F28016 DSP. I am suddenly started to get the following message when i connect to target:
Error connecting to the…
Other Parts Discussed in Thread: TMS320F28016 Hi,
I use a DSP TMS320F28016 as target and i use CCSv4 but i can't load program
I try to load a example project (gpio configuration)
the error is this:
Loader: One or more sections of your program…
Other Parts Discussed in Thread: TMS320F28016 I need several functions from stdio.h, and before biting the bullet and rewriting them myself, I had a peek around. I discovered the existence of stdio.h and added "#include <stdio.h>" to my source file and…
Other Parts Discussed in Thread: TMS320F28016 , CONTROLSUITE Dear community,
I'm trying to get my Olimex XDS100V2 emulator to work with the Olimex TMS320F28016 board. As software I'm using the CCS5.3.0 (free version) and (since I assumed it would help)…
Other Parts Discussed in Thread: TMS320F28016 Hello guys,
I have a question concerning the adc behavior of the TMS320F28016:
With the ACQ_PS bit it is possible to extend the acquisition width depending on the ADC clock. Is this time completely available…
Other Parts Discussed in Thread: TMS320F28016 I'm finally set up to use CCS 5 as a full debugger, and I get a Windows crash and forced immediate (within one minute) reboot "most of the time" when I click the Termnate button (red square) in the debugger…
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
Hello,
Daryl Lee said: 1. When I plug the USB cable into the XDS100-V2, I don't get that warm little "thunk" sound indicating the device has been recognized and is usable.
I'd start with the below resource on XDS100;
http://processors…
Other Parts Discussed in Thread: TMS320F28016 , SPRC191 I am using CCSV4.1.2.00027 with Windows XP on an Acer Aspire 1 using a TMS320F28016 in the Olimex DSP board. interfaced using the Olimex TMS320-JTAG-USB XDS100, all seem to work ok!
loading and using…