Part Number: TMS320F28033 Hi Experts,
I am asking for my customer.
Phenomenon: Customer/They use F28033 to do PSU, and they do PWM init missed the TBCTR = 0x0000 in the all PWM module. When they tested the code under half load condition, PWM1 and PWM2 …
Part Number: TMS320F28033 Hi Team,
Our customer has an old project with TMS320F28033 microcontroller. He is using the XDS510 Emulator and CCS v.3.3 but when he tried to add the TMS320F28033, it is not in the list of devices as shown in the screenshot below…
Part Number: TMS320F28033 Other Parts Discussed in Thread: C2000WARE Hello:
I think I would like to ask about the I2C communication of TMS320F28033. enable the FIFO module, and the depth of the FIFO module is 4. According to the
following figure, the…
Part Number: TMS320F28033 Other Parts Discussed in Thread: TMS320F28035 Hi team,
Due to supply issue, my customer want to use TMS320F28035 replace TMS320F28033, I see at datasheet they have different flash, Apart from this difference, what other differences…
Part Number: TMS320F28033 Hi,
Recently, I start to work on the arc detection. I am new. Is there some exemplary projects or libraries for the arc detection? Are they still available for downloading?
Thanks a lot.
Part Number: TMS320F28033 Dear team:
Customer question: F28033's I2C has only 4-level FIFO, can it write two 8-bits addresses and two 8-bits data?
Will the slave address configured by I2caRegs.I2CSAR take up FIFO space?
Best regards
Part Number: TMS320F28033 Hi expert,
I have a customer want to test power drop down situation.
So they turn down the power from 3.3V to 2.8V.
I know the it is already lower than our recommended voltage.
At about 2.8V, the DSP will crash, and the output…
Part Number: TMS320F28033 Hi expert,
I have a customer meet similar issue like this post.
The device is F28033. It is occasionaly happened.
They also stuck at PLLLOCKS status check
they also use external oscillator. so they check the oscillator waveform…