Part Number: TMS320F2806 Other Parts Discussed in Thread: C2000WARE Hello, I tried to access SPI on CLA on TMS320F2806, but It hangs. My question is this can I access SPI and UART on CLA on this device? I am a beginner and I did not find any example to…
Part Number: TMS320F2806 Other Parts Discussed in Thread: CONTROLSUITE Hi team,
Does TI have any about the stepper motor reference design of the DSP solution? include sample code and schematic and EVM?
Part Number: TMS320F2806 We are using the 2806 processor and were wondering if it is possible to connect one of the timers to the NMI. Or is the NMI only able to trigger from an external pin?
Part Number: TMS320F2806 Hello:
In this document, it is stated that "Reference voltage" is negative : In Fig 7, Current Loop Control Model, Note below the model block diagram.
But is not visible anywhere!
Where is it and how does one derive…
Part Number: TMS320F2806 Hi Team,
Sometimes it is necessary for the motor to switch directions quickly and frequently, and a power dissipation circuit is necessary.
Where is it embodied in the hardware circuit design? (Like drv8301kit, boost8301)
--
…
Part Number: TMS320F2806 We are trying to do validation for the C2000 compiler and we use optimization level 4.
Can you give us an example code snippet that would be optimized by level 4?
We need a way to prove the setting is active.
Part Number: TMS320F2806 Hi Team,
What is the difference in HRCAP in normal mode and eCAP in F2806x?
Also in the data sheet, HRCAP switching characterstics says that, minimum input width needed is 58.33ns. Does this mean any signal with smaller pulse…
Part Number: TMS320F2806 Hello,
I have two questions regarding HRCAP in F2806x,
Is it possible to Enable both Rising edge interrupt and falling edge interrupt?
Can we call both LowPulseWidth0, and HighPulseWidth0 functions if we need to know the values…
Part Number: TMS320F2806
Hi Champ,
I am asking for the customer.
Customers use TMS320F2806.
Customer has developed a CAN-based bootloader program under CCS3.3 before, and there is no problem in using it under CCS3.3. But now it is found that the bootloader…