Other Parts Discussed in Thread: TMS320F2812 hi everyone, we are developing an application using TMS320F2812 dsp custom board. our main task is to read parallel data from 4 ch ADC(AD7865) we are using three of them and send the parallel data to 2 ch DAC…
Other Parts Discussed in Thread: TMS320F2812 Hello, I am using the following standard C functions in my code while using the DSP/Bios. I am not using these functions in an interrupt. My question is, are these functions thread safe? Is there a listing…
Other Parts Discussed in Thread: TMS320F2812 I am using CCSv4 with a TMS320F2812 under Windows 7. The error message in the subject line has come up on this forum numerous times in the past: - http://e2e.ti.com/support/development_tools/code_composer_studio…
I meet a question to demostrate Running an Application from Internal Flash Memory on the TMS320F2812 DSP by using SPRA958h in CCS3.3。I want to use SPRA958i (the lastest version in CCS3.3)to test it again, but I can't find SPRA958i in www.ti.com. Could…
Other Parts Discussed in Thread: TMS320F2812 I am attempting to port an application from RAM to flash for a TMS320F2812, using CCSv4 and want to understand the programming of the flash registers better than on my last pass. Document SPRA958K provides…
Other Parts Discussed in Thread: TMS320F2812 Hi, I am trying to use the eZ dsp TMS320F2812 board. I connected it to the computer through the parallel port. A
DC analog signal is provided to pin 2 of P9 (ADCA0) using a DC source.
The VREFLO (pin 18…
Other Parts Discussed in Thread: TMS320F2812 Hi, I am trying to use the eZ dsp TMS320F2812 board. I connected it to the computer through the parallel port. A DC analog signal is provided to pin 2 of P9 (ADCA0) using a DC source. The VREFLO (pin 18 of…
This is the first time i am trying to make connection, and till now i have not tried to replace the part. Shall i do so?
This is for your information:
i changed the external clock from 50MHz to 16Mhz, but no help.
I have provision for one parallel…
I forgot to tell that I wont perform the control of the motor . The task of the board will only the identification algorithm, but for this I would require processing speed to perform a lot of floating point multiplications fast as possible. Im not sure…
Other Parts Discussed in Thread: TMS320F2812 I am designing a board that will use the TMS320F2812 to control a power supply. It it critical to prevent pins attached to power devices from glitching, especially during power up.
With other micros, I had…