Part Number: TMS320F28235 Other Parts Discussed in Thread: C2000WARE from where i can learn ccs software ,coding and other things .
not able to find study material online .
as power electronics master student i need this for my project.
project is related…
Part Number: TMS320F28235
CCS Version: 6.2.0.00050
HOW TO SOLVE THIS ISSUE DURING BUILD THE FILE
error: unresolved symbols remain error: errors encountered during linking; "FEC_DAB.out" not built gmake: *** [FEC_DAB.out] Error 1 gmake: Target…
Part Number: TMS320F28235 Hello, I am investigating a failure case in my customer's application software. Then I want to know the detail of the below caution descrived in the errata document to know if the root cause of this failure is this caution…
Part Number: TMS320F28235-Q1 Hi,
Just one doubt, in which case, can RAM data be changed or lost?
We are facing some cases, which shows that, the only root cause could come from changed RAM data. And the RAM addree are in the first 4KW of RAM memory map…
Hi! I'm using F28235 and have a ram on Zone 0 (location from spec = 0x4000). however, when I test the reading and writing of the data it does start at 0x4000 but at 0x4100. Why is there 0x100 offset (using mem bowser too)?
I have check schem and board…
Part Number: TMS320F28235-Q1 Other Parts Discussed in Thread: CONTROLSUITE Hi,
During CAN initialization, bit CCE (in register CANES) is 0, no mater CANRX is high or low.
From oscilloscope, CANRX pin is always highafter power on. Few times, there's a low…
Part Number: TMS320F28235 Hi,
Just one doubt about CAN module's TX pin, is it possible that, the TX pin can't output any signal in CAN mode, but can output signal when configured as GPIO output?
On customer's board, CANB module can receive message…