Part Number: TMS320F28374S Hi team,
Use SCIB for 485 half-duplex transmission, SCIB does not use interrupts, the main flow always queries, and the baud rate is 115200. The upper computer (PCs) periodically sends one byte of data to the TMS320F28374S…
I tried to use the Self-Test Application example code and have some questions about " STA_RAM_LOGIC_TEST " and " STA_RAM_DETECT ".
1. Is STA_RAM_LOGIC_TEST and STA_RAM_DETECT can work on RAM_M1 which be allocated to .stack in memory map?
(address…
Part Number: TMS320F28374S Hi team,
Follow the steps provided to port the APIs, which are verified when the code is migrated.
A sin wave with an input frequency of 50 Hz and a Vpp of 3 V. The RMS and average values of the AC voltage are found not…
Part Number: TMS320F28374S Hello,
I am using an TMS320F28374S and have currently the problem, that there is no more memory available for the CLA.
I assigned LS1-LS5 to the CLA as data memory (which are working to capacity) and LS0 as program memory…
Part Number: TMS320F28374S Hi Team,
There's an issue from the customer need your help:
I would like to ask about the increase and decrease counting problem after phase shift synchronization between EPWM modules.
Regarding this problem, the chip…
Part Number: TMS320F28374S Each address is 16 bits of data. But the data length in HEX is calculated according to 8 bits, can it be calculated according to 16 bits?
That's weird, right?
Part Number: TMS320F28374S
1,EPWM8A, EPWM8B,EPWM9A,EPWM9B,EPWM10A,
Can the five ch BST be set to send waves with a difference of 72 degrees?
2,EPWM8A and EPWM8B, that is, BST1 and BST3, have a difference of 144 degrees. How to set?
Part Number: TMS320F28374S Other Parts Discussed in Thread: SYSCONFIG , C2000WARE We use TI DSP TMS320F28374S to drive an LLC converter with Buck-Boost stage
During operation, we need to change switching frequency on the fly. For that reason we want…
Part Number: TMS320F28374S Dear team:
Do we have example routine for DCAN communication with FIFO enabled?
If not, My customer wants to know how to configure DCAN information to avoid the loss of DCAN information due to untimely query if DCAN communication…
Part Number: TMS320F28374S When configuring three-level wave generation, CMPA and CMPB(complementary) configurations are used. It is found that the tube is always on (or off), there is an exception, and there is no corresponding complementary. Are there…