Part Number: TMS320F28375S Other Parts Discussed in Thread: C2000WARE Hello Team,
can you please suggest me which tool is required to program and debug for TMS320F28375SPZPQ mcu?
thanks and regards Muzammil Qureshi
I already have to this and unfortunately nothing happen. Can check by trying this by your own. If you can do this, can you tell what exactly you've done to achieve this ?
Thank you.
Stephane Bonnot
Hello Allison,
Thank you for your continuous support, i really appreciate it.
Allison Nguyen said: Looking at the device.h file, the project must accidentally be pulling in the F2837xS ControlCard default configurations, which uses a 20MHz OSC source and…
Part Number: TMS320F28375S Hello Team,
I am working on TMS320F28375S with ccs 12.6.0 version. i have launchpad F28379D for use. I want to read the adc data in CLA. for that, i have made a function "uint16_t IoADCA_tReadSingleChannel(uint16_t adc_socnum…
Part Number: TMS320F28375S Other Parts Discussed in Thread: SYSCONFIG Hello Team,
I am using ccs 12.6.0 with sysconfig 1.19.0. I want to use FreeRTOS in my project. i am new to this controller. can you please help me with how to start with FreeRTOS in…
Hello Amir,
Omer Amir said: Are you excluding the linker command file which is not in use when building for RAM vs Flash?
yes, I am doing the same but still gives me the error (which i have shown previously) while building in flash. while building in…
Hello Siddharth,
Siddharth Deshpande said: What is the issue that you are facing while running from Flash?
I am not able to biuld my code in flash. i included the flash cmd file and excluded the RAM cmd file still i am not able to build the code in flash…
Hi Muzammil,
Now that your code is able to compile after editing the linker file, what behavior do you see when attempting to write to flash? Are you following the flash initialization shown in the flash_programming example for F2837xS?
Kind regards, …
Part Number: TMS320F28375S Hi Allison Nguyen ,
The LSPCLK related dividers are same for both FLASH and RAM i.e. SysCtl_setLowSpeedClock(SYSCTL_LSPCLK_PRESCALE_4), and there are not any initialized constants in RAM.
Thank You.
Arun Badiger