Part Number: TMS320F28376D Other Parts Discussed in Thread: SYSCONFIG Hi I want when e0 event is triggered, HLC generate an interrupt to call the function for resetting the CLB.
I don't know how I should implement it, I appreciate if someone guide me through…
Part Number: TMS320F28375D Other Parts Discussed in Thread: SYSCONFIG , CCSTUDIO , TMS320F28379D , TMS320F28069F , TMS320F28335 , C2000WARE java.lang.NullPointerException at com.ti.common.project.core.util.CTIProjectCoreUtils.getConfigurationSettings(CTIProjectCoreUtils…
Part Number: TMS320F28376D Hi team,
Can I use XDS100v2 with TMS320F28376D? If not, then could you share debug probe list that can support TMS320F28376D?
Best regards,
Kurumi
Part Number: TMS320F28376D Hi team,
When using USB module, I believe we need 60MHz on AUXCLKIN. Is there accuracy requirement (such as >± XXppm) for the external oscillator than can be used for this 60MHz AUXCLKIN?
Best regards,
Kurumi
Part Number: TMS320F28376D Hi team,
The TRM states that the USB module requires a fixed 60 MHz clock for bit sampling. However, the datasheet states that the range for f(auxpll) is 2-60MHz.
Does that mean we should set AUXPLLCLK= 60MHz exactly to use…
Part Number: TMS320F28376D Hi everybody
MCU runnig std alone out of flash and exectuing Boot in rom first
does the ROM boot takes care of RAM Init to 0x00 ?
or shoudl I init in my code to needed value ? in this case any compiler option to avoid writing…
Part Number: TMS320F28376D Hi team,
My customer would like to control chip-select’s EMxOE Timing (STROBE) by external signal. In this case, we can apply external signal to EMxWAIT pin, correct?
Also, when extending EMxOE STROBE period by WAIT signal…
Part Number: TMS320F28376D Hi team,
Can I confirm if TMS320F28376D can support USB2.0 high speed, or not? Datasheet mentions full-speed and low-speed only.
Best regards,
Kurumi
Part Number: TMS320F28376D Hi team,
For the Buffered DAC Electrical Characteristics of TMS320F28376D, are below gain and offset error values identical for each pcs?
For example, assuming the offset error was 8mV for 1 st powering up cycle. Then, is it…