Part Number: TMS320F28377S Hi Team,
Can you please share me the reason for the below issue while I am trying to instrument the software build on RTRT Version 7.5.0.0
FileA.h consists of the below piece of code. #ifndef EALLOW #define EALLOW __asm(" EALLOW…
Part Number: TMS320F28377S Hi,
While testing our product which uses TMS320F28377S microcontroller, we noticed that the ERRORSTS pin goes high. We saw in the NMI Shadow Flag Register (NMISHDFLG) that a Flash Uncorrectable Error (FLUNCERR) occurred.
The…
Part Number: TMS320F28377S Hi, My customer directly connected DAC outputs to ADC inputs on their PCB. Then, they observed glitches on these signals at ADC sampling rate. In below waveform, DACOUTA is connected to ADCIN15 DACOUTC is connected to ADCINC4 DACOUTB…
Part Number: TMS320F28377S 1. GPIO75 controls a switch connected in series to the F28377 power supply, with the high-level switch closed and F28377 powered; Low level switch disconnected, F28377 power off;
2.The problem I encountered is that I want the…
Part Number: TMS320F28377S Hi there,
We have manufactured a PCB with a TMS320F28377S processor for about 5 years. The board uses a CAN bus to communicate with other parts of the system. Part of the board test process is to test whether the CAN bus is…
Part Number: TMS320F28377S Hi Team,
GPIO84 is used as SCI boot, and should pull up to High because of SCI boot mode, Does the below design can achieve SCI boot?
After SCI boot, we need to config GPIO84&GPIO85 for SCIA function, Does the below design can…
I am unable to comprehend your issue.
AE_EE said: In the CS114 test, we see that the data produced by the MCU using the ADC readings is zero. This situation cannot be corrected without resetting the board or reinstalling software. The corrupted data is…
Part Number: TMS320F28377S Other Parts Discussed in Thread: SYSCONFIG , , TMS320F28379S Hi Experts,
I am asking for my customer.
we want to migrate from F28377D to F28377s.
Switch F28377s below. You can try it below, these F28377s, F28376s, F28375s, F28374s…
Part Number: TMS320F28377S Other Parts Discussed in Thread: C2000WARE Dear Champs,
I import the project in CCS12.4:
C:\ti\c2000\C2000Ware_5_01_00_00\device_support\f2837xs\examples\cpu1\F2837xS_sci_flash_kernel
And there shows the following errors, it…
Part Number: TMS320F28377S Other Parts Discussed in Thread: C2000WARE I want to use Cycle by cycle trip zone for tripping pwm pulses in TMS320F28377S. I tried using the example code, As mentioned in example code we need to nitially tie TZ1 high. and Pull…