Part Number: TMS320F28379D Other Parts Discussed in Thread: C2000WARE
I am getting fatal error whenever I am including the f28379D.h
Can you please help me?
Thanks in Advance!
Hi Soham,
I added EPWM4 to the example 2 updown aq and verified I can see EPWM4 functioning the same as EPWM3 for the example, with them both updating CMP values in an ISR. I assume this is what you did as well (and then modified it so the ADC results…
Prosen Dey said: GPIO mapping is also done properly as you have pointed out in your video.
For GPIO re-mapping, please stick to the instructions in SPRACE5. The video was made for F280025, a different device (although the concepts are still the same). …
Part Number: TMS320F28379D Afternoon,
My error reads as below:
"../2837xD_FLASH_lnk_cpu1.cmd", line 89: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated…
Part Number: TMS320F28379D Hi,
I am working on a C2000 to integrate with HIL. The microcontroller is supposed to be a mc for inverter. The AC frequency of the signals that are being read by ADC's is 500 Hz. I have used this setup but it was for 60 Hz…
Part Number: TMS320F28379D Other Parts Discussed in Thread: C2000WARE Resource Description Path Location Type #error directive: "You must define CPU1 or CPU2 in your project properties. Otherwise, the offsets in your header files will be inaccurate."…
Part Number: TMS320F28379D Other Parts Discussed in Thread: C2000WARE , SYSCONFIG Description Resource Path Location Type #1965 cannot open source file "F2837xD_device.h" main.c /LED_Blink line 6 C/C++ Problem
This is the problem statement.
I…
Part Number: TMS320F28379D Other Parts Discussed in Thread: C2000WARE I have a doubt regarding the i2c block set present inside the simulink under the package embedded coder support for Texas instruments C2000 DSP. I want to use the I2C module (either…