Part Number: TMS320F28384D Hello,
I would like to ask for a support.
For the microcontroller TMS320F28384D, I am looking either for its CAN controller compliance certificate to ISO 11898-1, or a test report, or a document that would show CAN tests…
Part Number: TMS320F28384D Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi all,
Relatively new to the embedded world, so forgive me for any oversights here.
Recently we have started using the CM core for our project. We have encountered…
Part Number: TMS320F28384D Hi champs,
When enable MPU function, we can use the PRIVDEFENA bit of MPU_CTRL register to switch privileged and unprivileged mode, is it correct?
However, it looks like CM4 cannot execute the application code if we enable…
Part Number: TMS320F28384D Hello,
In my project, I have a periodic ADC interruption that triggers two tasks: a CPU1 task and a CLA1 task. This is what the functions look like:
__interrupt void INT_myADC0_1_ISR()
{
// Cla1Task1() is triggered in…
Part Number: TMS320F28384D Regarding the secure flash boot feature present on TMS320F2838x devices, Does a CMAC-based secure boot offer good security? How do you ensure that the keys are not stolen or misused? If I purchase this development board, what…
Part Number: TMS320F28384D Other Parts Discussed in Thread: UNIFLASH
Tool/software:
We have been using the 2837xD family for many years, and recently received our first prototype boards with the 28384D. We're struggling with being able to consistently…
Part Number: TMS320F28384D Other Parts Discussed in Thread: C2000WARE , SYSCONFIG Hello,
I have a question about the EMIF examples for this launchpad. I need to connect a 16 bit nor flash chip to the launchpad (i also have a stand alond controller on…
Part Number: TMS320F28384D Dear TI community,
I am using an eCAP module to observe and check the generated signal of an ePWM module via the X-BAR. (example ecap_ex2_capture_pwm.c as basis)
After setting everything up (4 capture events to observe the…
Part Number: TMS320F28384D Previous topic(resolved) but the same project:
TMS320F28384D: The compiler for IEC 61508 SIL-3 certification - C2000 microcontrollers forum - C2000 ︎ microcontrollers - TI E2E support forums
Hello,
I use ARM TI CGT CQKIT…
Part Number: TMS320F28384D
Hi champs,
In our latest version (ver. E) of data sheet, we add one 2.2Kohm pull-up resistor to JTAG TMS pin.
Some of my customers use F2838x devices and the projects are already in production, is there any side effect…