Part Number: TMS570LS0714 Hi Team,
There's an issue from the customer need your help:
Hello:
I want to make a BOOTLOADER for TMS570LS0714APZ. If I use the same program but different ICs, I will find that some can be programmed successfully, but…
Part Number: TMS570LS0714 Other Parts Discussed in Thread: HALCOGEN I am trying to use the FreeRTOS methods from Halcogen.
I am using Halcogen v04 07 01. I started with the project for Free RTOS : TMS570LS0714PGE_FREERTOS.
I have left settings related to…
Part Number: TMS570LS0714 I would like to use this pin as an interrupt source.
I don't want it to trigger an actual ISR but I instead to poll the interrupt flag to see if there has been an event.
The reason is that the external signal is very spurious…
Part Number: TMS570LS0714 Hi TI Team,
I would like to program the TMS570LS0714 via JTAG by using our own programmer.
I used the CCS to build a bootloader and wrote the bootloader to sram of TMS570LS0714. I used the bootloader to call the API to program…
Part Number: TMS570LS0714 The only description I can find about what the nRST (warm reset) resets is in the "Cortex-R4 and Cortex-R4F Reference Manual" which just states that "This signal is the main processor reset that initializes the majority of the…
Part Number: TMS570LS0714 Other Parts Discussed in Thread: HALCOGEN , TMS570LS0914 Hello all,
I want to generate a pwm signal (~60kHz) on the multiplexed pin 12 on TMS570LS0714APZ. This pin's default function is GIO.
I referred some articles to generate…
Part Number: TMS570LS0714 Hi
We have a project based on TMS570LS0714, where a certificate for compliance with ISO13849 is required. The assessment company is requesting information for which we need the FMEDA. I am aware of that some paper was made some…
Part Number: TMS570LS0714 I want to connect an always enabled watchdog to nRST, but will this prevent me from using JTAG for programing and debugging?
If so I’ll have to find a way to disconnect the watchdog output from the nRST input, but I would prefer…