Part Number: TMS570LS1115 1.What is the tolerance range of the external pin filter capacitor for tms570ls1115 chip 1.2V core power supply?
2. Is there no requirement for 1.2V and 3.3V power on sequence as stated in the specification?
Part Number: TMS570LS1115 Hi team,
Here's an issue from the customer may need your help:
During bench test, there is no problem with the small torque. High torque has the following error:
CAN communication is lost, supply current is reduced, ePWM…
Part Number: TMS570LS1115 Other Parts Discussed in Thread: TMS570LS1227
Hello,
I have the same problem at TMS570LS1227. Is there any progress on this issue?
e2e.ti.com/.../tms570ls1115-i2c-interrupt-not-working
Part Number: TMS570LS1115 Hi expert,
My customer is using MCAL on TMS570LS1115 device. They are informed of lacking LIC. Could you help us with this?
Thanks
Sheldon
Part Number: TMS570LS1115 Hi expert,
My customer met a clock failure issue.
For TMS570LS1115 device, Non-AUTOSAR version system.c from TI has some configurations on the MCU. In development process, we find system_init in _c_init00 and some other APIs…
Part Number: TMS570LS1115 Hi expert,
My customer is developing with TMS570 and they need latest version of MCAL which is complient to AutoSar.
Could you help me with that?
Thanks
Sheldon
Part Number: TMS570LS1115 Hi all,
For our project iam working on the CAN re-init after a bus-off situation. When bus-off happens a interrupt is given where i want to re-init the CAN so i can go back to bus-on mode.
Is it neccesary to re-init the whole…
Part Number: TMS570LS1115
Tool/software: Code Composer Studio
Hi expert,
My customer meet "Debug assertation failed" alert when build program, I have asked them to check any non-ASCII in PC name, workspace and source code but we didn't find anything…
Hi Gabriel,
Gabriel B said: This HalCoGen code you shared has an interesting implication.
Yes, you are right. There is a bug and please refer below workaround from QJ.
(+) TMS570LS1115: I2C interrupt not working - Arm-based microcontrollers forum - Arm…