Part Number: TMS570LS1224 Other Parts Discussed in Thread: SEGGER Hi all,
I am looking for the development and debugging tool for the both TMS570LS1224 (Launchpad evaluation) and STM32 Cortex M3( NUCLEO‑ evaluation ) .
Intend to keep it common tool as much…
Jens Benner said: thank you very much for your prompt reply. When writing to the bank 7 flash using Fapi_AutoEccGeneration mode and with a multible of 8 Bytes will the ECC bit automatically generated and will I get an exception during read when the ECC…
Part Number: TMS570LS1224 Other Parts Discussed in Thread: HALCOGEN Hello everyone, I have a question about the configuration of the stack for a TMS570LS1224 Hercules MCU. The stack configuration is based on the default settings in HALCOGEN. Furthermore…
Part Number: TMS570LS1224 HI
I currently working on TMS570LS1224, and try to erase flash memory using F021 FLASH API library but didn't erase, code will goes to prefetch entry.
and I am trying to erase at following address (0x000A0000).
Part Number: TMS570LS1224 Hello all,
I am working on a legacy Projekt with a Bootloader and Application. I had ported the Application to FreeRTOS wich runs fine so far when I run the Applcation right from the beginning of the Flash for simplifing debugging…
Hi Jens,
Can you please refer below thread once, this might be useful in this context:
(+) TMS570LS1224: FreeRTOS with FPU support - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums
-- Thanks & Regards, Jagadish…
Part Number: TMS570LS1224 Other Parts Discussed in Thread: HALCOGEN After converting the linker file of the ls12_can_boot project into an IAR file using the HALCogen tool as below, I created an additional F021_API part.
And as in the CCS environment,…
Part Number: TMS570LS1224 Hi,
I'm trying to flash an application via UDS which is in boot of TMS570LS1224.
In UDS I'm receiving the data via blocks, where max size of a block can be 4093.
So, if the data to be flashed is > 4093, it will be divided…
Part Number: TMS570LS1224 I need to Bring up the plain SCI (not Lin SCI) up, for printing debugging prints to Serial terminal.
Can i get a step to step guide, how to configure in Halogen or any working example will do.
I see examples given only for SCI…