Part Number: TMUX1511 Tool/software: Dear Forum Members,
I hope this message finds you well. Question 1: We conducted a test where we allowed a larger current to flow from source to drain when the TMUX1511 switch was ON, anticipating an abnormal current…
Part Number: TMUX1511 Tool/software: Mux team,
A customer needs a mux for an RGMII interface. What is the best one to use? Is TMUX1511 is the right choice for this?
Thanks, Darren
Part Number: TMUX1511 Other Parts Discussed in Thread: TMUX136 Tool/software: Hello,
I have to do the same project but I am a beginner in PCB design. I just have one question about this project. If I have an SDI-3G signal at the input, will it work…
Part Number: TMUX1511 Tool/software: Hi team,
Would like to ask if TMUX1511 is suitable? It is used for 66MHz eSPI (bi-directional) and 66MHz SPI (uni-directional).
Thanks!
Best regards,
Alice Fan
Part Number: TMUX1511 Tool/software: Hello,
I seems the datasheet of the TMUX1511 is not available on your Web site. Could you correct this please?
Best regards,
Part Number: TMUX1511 Other Parts Discussed in Thread: TMUX6211 , TS5A22362 Tool/software: Hi,
Customer is finding the device to support -1V with similar specification to TMUX1511.
I found TMUX6211 but it's quite expensive compared to TMUX1511.
…
Part Number: TMUX1511 hi,
Fout2 inputs a frequency square wave from 10KHZ to 100KHZ, and SEL1 and SEL2 are both high or low levels. SEL3 and SEL4, due to the connection of inverters, have opposite levels to SEL1 and SEL2. When SEL1 and SEL2 are high…
Part Number: TMUX1511 Other Parts Discussed in Thread: TMUX1574 Hello,
I have downloaded IBIS model for TMUX1511 for Signal Integrity simulation.
However S1,S2, S3, S4 and D1, D2, D3, D4 pins are defined as inputs only.
As per datasheet and our…
Part Number: TMUX1511 hi,
When Fout2 connects signals from 10KHZ to 100KHZ, the measured TP10 and TP11 are a set of reverse frequency signals. A 1pf capacitor is welded at the position of C31, and the voltage TP13 0.0024V TP15 0.0015V TP16 0.0015V TP17…