Part Number: TMUX7213 Other Parts Discussed in Thread: TMUX6213 Hello,
We are using two TMUX7213s to switch signals driving and sampling two ultrasonic transducers. We drive one at a time and sample the other and then swap.
Some of the transducers…
Part Number: TMUX7213 Tool/software: i'm using TMUX7213PWR for one of my projects.
Could you please share the anolog input voltage thresholds for Low and High signal inputs on Sx, Dx, SELx lines?
I have pasted the below picture for your reference…
Part Number: TMUX7213 Dear Specialists,
My customer is considering TMUX7213 and has a question.
I would be grateful if you could advise.
---
TMUX7213 has a spec of break before make time.
Could you please the meaning of this spec.
BBM is generally…
Other Parts Discussed in Thread: TMUX7213 , TMUX7219 Hi Team,
Do we have solution that could replace DG403? ( https://www.vishay.com/docs/70049/dg401.pdf )
But the output voltage range is 17V~-13V
Roy
Part Number: TMUX1111 Other Parts Discussed in Thread: TMUX7212 , TMUX7213 , TMUX7211 Hi Team,
Could you please suggest a +/-20 V @5mA between drain/source bidirectional that can be controlled from a uCPU? Lower Ron is better.
TMUX1111 looks promising…
Part Number: TMUX1574
Tool/software:
Shoot-through current occurs when CMOS inputs are somewhere between their High and Low voltages, effectively turning on both MOSFETs in the CMOS structure. In many devices, including analog multiplexers, this creates…
The following table helps select th e right multiplexer and switch with Mid Voltage 25V =< VSIGNAL =< 99V in different configurations:
Precision , Protection , Automotive , Extended Temperature
Configuration
16:1…