Part Number: TPA3101D2 Other Parts Discussed in Thread: AM625
Hi
I need to added the 10W + 10W Audio Amplifier circuit to AM625 controller as given in block diagram along with Line In and Audio Head Phone Jack .
Please verify the circuit
Regards…
Can I use TPA3101d2 with an audio speaker whose rating is 4W on the input for continuous use which would be a 5.66V sine wave in practical usage if not please suggest some method of controlling the output of the audio for the above purpose like decreasing…
Other Parts Discussed in Thread: TPA3101D2 Hi,
I want a stereo audio amplifier with output power of 4 watt on each channel. My speaker specs are 5 watt max power, 8 ohm.
TPA3101D2 gives continuous output power of 10 watts. I want to know, is there…
Hi~
Our cuasomer will use External MUTE Control for TPA3101D2PHPR(HTQFP). If see data sheet..
If external MUTE control is desired, and automatic recovery from a short-circuit event is also desired, an OR gate can be used to combine the functionality…
Hi Jerry,
It depends on your application needs. For the USB interface you can use PCM290xC family, PCM2912A or PCM270xC family.
For the Class-D you can choose one from the TPA family, I have tested PCM2906C and PCM2912A EVM's with TPA2025D1 and TPA3101D2…
Hi, Shankar,
I would recommend to take a look at the TLV320AIC32 and TLV320AIC3101. These devices support headphone and line outputs. Additionally, the line outputs can be connected to an external Class-D amplifier. However, they only support 8-ohms…
Other Parts Discussed in Thread: TPA3106D1 , TPA3100D2 , TPA3101D2 Dear All...,
I really looking a complete circuit diagram for TPA3106D1 IC. Pls forward me if any one is having. It's not that which is in Texas data sheet.
Rohitha
Other Parts Discussed in Thread: TPA3100D2 , TPA3101D2 The TPA3100D2, TPA3101D2, and TPA3106D2 have SYNC terminals which allow the internal oscillator to be sync'd up with a second device, or your SMPS.
The data sheet describes how to use this, but…