Part Number: TPA3110D2 Hi,
We use the TPA3110D2 for the loudspeaker, and now, we power on but there are the c urrent noise, please kindly review the schematic diagram and provide your commend if there are any error, thanks.
NTB-A100.pdf
Part Number: TPA3110D2
Hello team,
I'm using the TPA3110D2 for one of my client projects., I noticed that when I power on the circuit and play any audio, the speaker initially produces a POP( sounds like TUK) with a large current consumption. Then…
Part Number: TPA3110D2 No audio output from TPA3110D2.
Hello TI,
I'm making a circuit using TPA3110D2, in PBTL configuration.
I saw that is necessary to keep the pin SD at least 2V to keep it in HIGH position, but using the 100K resistor that is showed…
Part Number: TPA3110D2 combinepdf.pdf
Hi Team,
I'm using the TPA3110D2 for one of my client projects. We're employing this chip for 2 x 15W audio amplification, with input coming from the Realtek audio codec ALC5616-CGT. However, the TPA3110D2 isn't functioning…
Part Number: TPA3110D2 Hi,
We are developing custom board for one of our client(Audio application).We are using TPA3110D2PWPR Audio amplifier to connect with two 10W speaker.
Below is the issue which we are getting when we powerup the board and send the…
Hi Sir,
We found that there is a POP noise when the SD# PIN is enabled.
We attempted to connect an SD# to a button for control. Whenever PVCC and AVCC are active, regardless of when I enable the SD# PIN, it results in a POP noise.
Can you provide suggestions…
Part Number: TPA3110D2-Q1 Hi,
For TPA3110D2-Q1, doe it can support 8ohm load speaker?
Or TI have other ~10W stereo Class-D AEC-Q100 amp can support 8ohm?
Thanks!
Jeff
Part Number: TPA3110D2 Hi,
Could you please review the design of the schematics attached?
I have attached two sheets. The first sheet shows the part being used as a 10W Amplifier for calling purposes. Here, only 1 channel is used. So, is it okay to leave…
Part Number: TPA3110D2 Hi,
Could we provide the chart of THD+N vs output power at VCC=12V and RL= 4Ohm application?
Target output tis 15W and want to check its THD+N performance.
Thanks and Best regards,
Tiger
Part Number: TPA3110D2 Schematic_SIF (1).pdf
The IC#TPA3110D2 placed at Legends U23 & U24 in the attached pdf is working for single channel . The output requirement is amplified Sine Wave. Not getting the required amplified Sine wave output. There is…