Part Number: TPA3116D2 Hi,
I'm working on the TPA3116 amplifier. Config : Gain = 26dB, PVcc = 24V, RL = 2 Ohms, in PBTL mode.
- I'm able to have +90W but with THD = 7-9%. Is it normal to have that much THD to obtain near 100W ?
- Is the initial…
Part Number: TPA3116D2 Dear TI experts,
My customer considers TPA3116D2 for their new project, and they have a question about BD/1SPW modulation.
BD modulation is described as follows in the datasheet;
- This is a modulation scheme that allows operation…
Part Number: TPA3116D2
TI Team, The data sheet for these devices mentions that it is customary to tie the AVCC pins and PVCC pins together on the board to the same voltage net. However, what happens if we don't tie them to the same net? We can see in…
Part Number: TPA3116D2 Other Parts Discussed in Thread: TPA3255 , TAS5828M , TAS5827 , TAS5805M Hi!
I am planning an experiment where I need to "play" white noise into coils, in order to create a short ranged multi frequency electromagnetic field.…
Thank you,I successed in connecting the tpa3116d2 to adc5311.
I I wanna produce a current source-the power is 40w,the higher frequency is 650khz,the lower frequency is 150kHz,the voltage requires 5V. The current looks like in the figure.
I wanna kown…
Part Number: TPA3116D2 Hello, In order to better understanding of the TPA3116D2 functional block. I would like to ask why there isn't the pin 1 (MODSEL) on the functional block. And also, why is GAIN pin seems duplicated?.
On the other hand, and just…
Part Number: TPA3116D2 Hi,
I want to use the TPA3116D2 amplifier to output a minimum of 50W at frequencies in the 20-30kHz band with a 1Vrms input signal, 4 Ohms load.
After various tests in PBTL mode, my output signal saturates as soon as 0.7Vrms, and…
Part Number: TPA3116D2 The inductors and ic on the mono subwoofer channel (PBTL) om my dual amplifier board are very hot. The stereo high end amp is much better and only gets warm. I measured the idle power and it’s 10W. (19,5v 0,5A) . The stereo amp…