Part Number: TPA3130D2 Other Parts Discussed in Thread: PCM5121 , TAS5825M , TAS5805M Hi,
We are using TPA3130D2DAP in our design with 15V supply. We are using MCU 3.3V logic and we would like to control TPA3130 via 3.3V MCU IOs. Please answer the following…
Hi Thomas
Thomas Durey said: Will it cause some problem ? Like saturation or clipping ?
If you still gives maximum input level, the output will clip. You mentioned max input is 1.5V peak, 20dB Gain should get 15V peak output, but your supply voltage only…
Part Number: TPA3130D2 On page 26 of the TPA3130D2 datasheet, the diagram of a typical application is given with two amplifiers. To synchronize the two amplifiers the sync pin is used through an RC circuit.
We have implemented this scheme (dual amplifier…
Part Number: TPA3130D2 Hi Sir,
As title, I would ike to know if TPA3130D2 support 2x15W (stereo)@4ohm, 12V? In this condition, the current would be up to 4A (IC OCP is 4.5A ) any themal concern?
Thanks,
Jacky
Part Number: TPA3130D2 Other Parts Discussed in Thread: TPA3116D2EVM hi all,
IC: tpa3130d2 PVCC and AVCC = 15V
BD mode, there is no input audio, and the oscilloscope tests any output (single end to ground test) DC = 7.5V, which I think is correct.
1spw…
Part Number: TPA3130D2 Hello Sir:
Can we use TPA3130D2 to replace AP2622??
Do you have better solutions?
The first element is lead time should be short and secondary is price.
Please help to provide recommendations for us.
Thanks a lot.
Part Number: TPA3130D2 Hi team,
One of our customers needs the RθJC (Junction-to-case thermal resistance) and RθJB (Junction-to-board thermal resistance) when doing thermal simulations, but they are not described in datasheet. Can I ask if there is any…
Part Number: TPA3130D2 Now a project is using a Class D power amplifier chip, model TPA3130D2.The design adopts Mono Mode configuration, which can provide 30W.Use 24V@2A adapter for power supply.
Problem: There is instantaneous power consumption greater…
Part Number: TPA3130D2 Hi Sir,
To measure the TPA3130 output for mono woofer application, it is found that the speaker output have an audio 117KHz output without input signal.
when playing 200Hz sound, 117KHz will also be loaded on it
The attachment…