Part Number: TPA3136D2EVM Other Parts Discussed in Thread: TPA3136D2 Hi,
From my recent thread about the audio demo,
While some switching noise is acceptable on one end of the resistive load, I'm seeing nearly
1 V p-p switching noise on the output…
Part Number: TPA3136D2EVM Other Parts Discussed in Thread: ALLIGATOR , TPA3136D2 Hi,
I am working on the audio demo using the TPA 3136D2 EVM. The load is a
PBTL mono load.
I am using a 4 Ohm 3W resistor for this, resistance measures 4 Ohm on a multimeter…
Part Number: TPA3136D2EVM Other Parts Discussed in Thread: TPA3136D2
I had one last question about the single ended p-p voltage measured across
the resistive load.The load is 4 Ohm, 3W. The max p-p voltage across the
load should ideally be 9.78 V. This…
Part Number: TPA3136D2EVM Other Parts Discussed in Thread: TPA3136D2 I found a function generator and had the soldering changes implemented on the TPA3136D2 EVM to configure
it for a mono output. The function generator struggles to consistently maintain…
Part Number: TPA3136D2 Hi !
TPA3136D have POP noise when power up and power down ,Pull up and pull down the SD pin have POP noise too. the SCH is the same as TPA3136D2EVM, How can reduce it ? Many thanks !
Part Number: TPA3136AD2EVM Other Parts Discussed in Thread: TPA3136D2EVM Hi,
In the TPA3136D2EVM, what is the reason for using electrolytic capacitors for parts C2 and C8? Their
value is 100 uF. If they are replaced by ceramic caps, their sizes will get…
Part Number: TPA3136D2 Today the audio demo using the Colibri 3.2 eval board and the TPA3136D2EVM worked
with the single 4 Ohm 3W loudspeaker.
The max analog headphone volume for the SGTL5000 audio codec is 12dB and the
TPA3136D2 has a fixed analog…
Part Number: TPA3136D2
The input to the TPA3136D2 is coming from the analog headphone output of the SGTL5000 audio codec.
I have used a combination of the TPA3136D2EVM schematic and Fig 19 from the TPA3136D2 datasheet
to put this schematic together.…
Shawn, Still waiting for your help. I set the voltage at the PLIMIT pin to 1.25V on the TPA3136D2EVM. The sound coming out of the analog headphone output has been set to 12dB (max possible from SGTL 5000 codec from the colibri 3.2 eval board). The…
Hi, Satoshi
You can reference TPA3136D2EVM for single ended input design, the EVM support single ended input. TPA3136D2 support BTL/PBTL output, if you need to support single ended output, you can reference TPA3121D2EVM schematic, for the DC blocking…