Part Number: TPA4860 Hi,
As far as the TPA4860 datasheet is concerned, there is no information on thermal resistance (θJA, θJC, θJC(top), etc.). https://www.ti.com/jp/lit/ds/symlink/tpa4860.pdf
Is there any information you can provide?
Thanks, …
Part Number: TPA4860 Other Parts Discussed in Thread: TPA2005D1 , TPA6205A1 , TPA2008D2 I need an audio amplifier, for human voice frequencies.
1 channel.
8 Ohm load impedance.
1-2 Watt.
Is TPA4860 is the right solution?
Part Number: TPA4860 Customer design for the TPA4860 has a 0.1uF/25V ceramic cap as well as a 33uF/25V tantalum capacitor on VDD (pin 12). VDD = 5V.
Due to tantalum sourcing issues, they would like to replace these with alternate ceramic caps: 0.1uF…
Other Parts Discussed in Thread: TPA4860 Hello there guys,
Could anyone tell if it is possible to have a amplifier with gain less than unity? Specifically, if TPA4860 allows gains smaller than 1?
In my application, I'm driving a speaker (8ohm) to…
Hi, Kai,
I will verify this on our evaluation modules.
We also have an alternative, the TPA4860. Please take a look at the figure 18 of datasheet for details. The single ended output can reach up to 250mW with an output load of 8ohms and VDD = 3.3V…