Part Number: TPD1E05U06 The ESD device is connected to the circuit in parallel, as shown in Figure 1. When ADS is used to simulate IL, circuit diagram 2 is built in parallel mode, and the simulated IL is shown in Figure 3. On the contrary, the circuit…
Part Number: TPD1E05U06 Hi All,
The same as the title, is it correct that using DMM meter diode mode to confirm ESD component is damaged or not? And how to measurement?
Part Number: TPD1E05U06 Other Parts Discussed in Thread: TPD4E05U06 Hi Team,
We use TPD1E05U06RVZR for USB3.0.
Then, we don’t use D3- and D3+.
Therefore, those pins is connected to GND.
Is my understanding correct?
<Image>
Regards,
Hid…
Part Number: TPD1E05U06-Q1 Hi Team,
There is a good new that we could DIN TI product!
Customer is looking for the TPD1E05U06QDPYRQ1 free sample for prototype build!
But TPD1E05U06QDPYRQ1 is out of stock, May I know the difference between TPD1E05U06DPYR …
Part Number: TPD1E05U06-Q1 Hello Team,
My customer wants to know how much capacitance value when Vio set to 0V.
The datasheet mentions DPY package IC has 0.42pF at Vio set to 2.5V.
However, no data at Vio set to 0V.
could you please provide capacitance…
Part Number: TPD1E05U06 Other Parts Discussed in Thread: ESD401 , TPD2E009 Hey team,
Hope everyone's having a great day. I need a drop-in for PESD5V0X2UAM ( webpage & datasheet ), which I doubt is available but if I could at least get some recommendations…
Part Number: TPD1E05U06-Q1 Dear team,
My customer uses this device for USB 2.0 interface. H3 and H4 are two USB pins. The CAR OEM has a requirement that they need to test LCR of USB signal pin before and after ESD test(power down mode), and then make …