Part Number: TPD1E10B06-Q1 Other Parts Discussed in Thread: ESD2CAN24 Hi team,
When I learned TPD1E10B06-Q1 DS, I found that the SPEC is related to the test method. could you pls help confirm the following question.
1. Does TI’s bidirectional ESD have…
Part Number: TPD1E10B06-Q1 Hi,
Please share the MTBF and FIT of TPD1E10B06QDPYRQ1
The following link does not include TPD1E10B06QDPYRQ1, but there is one for PTPD1E10B06QDPYRQ1. I would like to inquire whether these two are the same?
Thanks
Part Number: TPD1E10B06-Q1 Hi team
There is a good new that we could DIN TI product!
Customer is looking for 5V ESD
It seem TPD1E10B06-Q1G could meet customer requirement!
Please help suggest TI solution, THX
Other Parts Discussed in Thread: TPD1E10B06-Q1 , TSM24CA-Q1 , ESD2CAN24-Q1 Hi Team,
Could you pls help recommend an auto alternative for MLSEP05A-0402, SMBJ30CA, WPE24CT23BL-G? Thanks!
Regards
Hailiang
Part Number: TPD1E10B06-Q1 Other Parts Discussed in Thread: TPD2S701-Q1 , TPD2S703-Q1 Hello,
My customer is asking if we had any I/O protection solutions for transceiver interfaces (e.g. CAN, LIN, 100/1000BASE-T1) that connect to automotive wiring harness…
Hi Matthew,
Glad to hear your other design is completed! I would recommend TPD1E10B06-Q1 if you need an auto-qualified device. Please see the table below:
TSD05C
TPD1E10B06
Vrwm (V)
5.5
5.5
Package Type
SOT
SOT-5X3 (or W1SON)
Package Size (L…
Below are the latest recommendations of devices for multiple interfaces that provide you IEC protection and paired with low capacitance that minimizes impact to bandwidth in the system. Please also refer to our System-Level ESD Guide for more details…
Part Number: TPD1E10B06 I am developing a product using TPD1E10B06DPY, High temperature and high humidity (65°C 98%) operation test, problem occurred at about 80Hr.
I measured both ends of the diode where the problem occurred with a DMM, The resistance…
Part Number: TPD1E10B06-Q1 Dear all
Could you tel me the products that are most suitable for LIN?
Specification Automotive Grade Use only LIN 1ch
Masa0301
Part Number: TPD1E10B06-Q1 Other Parts Discussed in Thread: TPD1E10B06 , STRIKE
When I read TPD1E10B06 datasheet, I can't understand what is the DC breakdown voltage. And what is the difference between DC breakdown voltage and clamping voltage? when will…