Part Number: TPD4E05U06-Q1 Other Parts Discussed in Thread: TPD4E05U06 Hi Team,
We are using the part TPD4E05U06, but there is only s2p model available for this part in website. We need this ESD to be used in our simulation. How to use it for differential…
Part Number: TPD2E2U06-Q1 Other Parts Discussed in Thread: TPD2E2U06 , DP83TG720EVM-MC , TPD4E05U06-Q1 Dear team,
Is TPD2E2U06(-Q1) usable for 1000base-T1 ESD suppressor diode? I feel line capacitance CL=1.5pF is quite high for 1Gbps signal.
But DP83TG720EVM…
Part Number: TPD4E05U06-Q1 Other Parts Discussed in Thread: TPD4E05U06 I use ADS for simulation. I want to confirm whether TPD4E05U06-Q1 has S parameter data of *.s4p? I only found TPD4E05U06 S parameter: *.s2p.
https://www.ti.com/product/TPD4E05U06#support…
Part Number: TPD4E05U06-Q1 Hello, my co-workers are trying to understand how the PCB routing is done when using the TPD4E05U06QDQARQ1 in flow-through configuration. We have looked at Figure 13 but have differing opinions. Is it correct in saying that…
Back to Interface Home Page
DisplayPort Protection
Highlights:
Data speeds up to 20Gbps
8 data lines, 20 total pins
3.3V, 500mA Input
Low capacitance required on data lines
Device
V RWM
Cap
(pF)
ESD(kV)
IEC61000-4-2
Contact
No. of Chan…
Below are the latest recommendations of devices for multiple interfaces that provide you IEC protection and paired with low capacitance that minimizes impact to bandwidth in the system. Please also refer to our System-Level ESD Guide for more details…
Part Number: TPD4E05U06-Q1 Other Parts Discussed in Thread: TPD4E05U06 Hello, I'm a little confused how to wire up the TPD4E05U06QDQARQ1 to an RJ-45 connector for Gigabit Ethernet. Here is what I have so far:
I've been reading the datasheet and I…
Part Number: TPD4E05U06-Q1 Hi team,
My customer wants to know TPD4E05U06-Q1 N.C. pin capatitance value. The customer plans to connect the signal with N.C. pin so that the signal trace is straight.
Please let me know.
Best regards, Fumio Nakano
Part Number: TPD4E05U06-Q1
Hi Team,
I am seeking clarification on the N.C. pins of the TPD4E05U06-Q1. I realize these pins are to allow the signal traces to be straight through routing, but it is unclear 1) how they should be wired on the schematic and…
Part Number: TPD4E05U06-Q1
The datasheet for the part displays this pin out with pins 1 and 2 with D1+ and D1-. My question is - If one were to use pins 1 and 2 for a differential signal, with the positive polarity on pin 1 and the negative polarity…