Part Number: TPD8S009 Provide case details or comments: I wish to replace the obsolete CM1233-08DE from ON Semiconductor, datasheet attached, with the TPD8S009DSMR, if you can confirm it is functionally equivalent. I need help with the pin mapping in…
Part Number: TPD8S009 HI,
I'm using the TPD8S009DSMR and TPD4E1DRLR ESD protection for DisplayPort extender board.
I'am routed this board using DP layout constraints, but the board (DP) doesn't work !!
I suspect the ESD protectionsdiodes…
Hi Team,
TPS8S009 has optional VCC connection pin.
May I know, what is the purpose of this pin and when do we need VCC connection for ESD device in general case?
Thanks a lot!
Andrew
David
Thank you for answer.
I use the Ttype A of the main board, and I want to apply Type A, not Type B, to the board I want to make. Can I connect the lines like below?
Q1) A Connector TUSB1046 SSRXN(5) - SSTXN(7) SSRXP(6) - SSTXP(8) SSTXN(8) - SSRXN(4) SSTXP…
Other Parts Discussed in Thread: TPD8S009 Hello, For a high speed video display application, I am planning to use TPD8S009 between a LVDS connector and a FPGA. Am I right in saying that Vcc of TPD8S009 should be connected to the supply voltage of the corresponding…
Hi Team,
Is there any difference between Dx+ pin and Dx- pin? I consider to connect Dx+(Dx-) pin to Dx-(Dx+) of display port signal. I believe it is no difference between these pins.
Best Regards, Yaita
Other Parts Discussed in Thread: TPD8S009 HI,
I've been using the TPD8S009 ESD protection for DisplayPort applications running at RBR and HBR for a while.
Does this device also support the HBR2 (5.4 Gbps) bandwidth?
Best Regards,
Marco
Other Parts Discussed in Thread: TPD2E009 , TPD8S009 Team,
Customer is using the Aria II GX transceivers at 3.75Gbps. Will the TDP8S009 work at this speed? I've also shown the TPD2E009 but they prefer a multi-channel device. Please let me know or make…