Hello,
TPS55065-Q1 has output current of 0.5A where as TPIC74100-Q1/TPIC74101-Q1 have output current ratings of 1A. Between TPIC74100-Q1/TPIC74101-Q1, I do not think of any difference other than switching frequency.
If you look at below link, there is…
Hello Stefan,
Regarding the power converter. If you are expecting to see the full voltage range from 3.0V to 5.5V I would advise against a SEPIC topology.
You could look into the TPS55065-Q1 or the TPIC74101-Q1 to condition the wide input voltage to…
Other Parts Discussed in Thread: TPIC74101-Q1 , TPIC74101 If my driving voltage is 3v or less than 5V(minimum 3V) , does the tpic74101-q1 start and have self buck/boost transitioning? or should the start up voltage be always greater than 5V?
My input voltage…
Part Number: TPS55332-Q1 Other Parts Discussed in Thread: LM5121 , TPIC74101 Hi
I am using TP55332 IC for one of my application. The DC-DC converter is designed to operate as BOOST converter which provides 18.5V regulated output voltage from the input voltage…
Other Parts Discussed in Thread: TPIC74101-Q1 , TPIC74101 Is the tpic7401-q1 a buck - boost IC like LM3115-1 of linear technology or will it operate only in buck or boost mode ?