Part Number: TPL0202-10 Hello Team,
can you confirm that the high level voltage for SCLK, DIN, CS can be 5V even if Vdd=3.3V, please?
According the data sheet this is not really clear to me.
According to Abs Max Ratings: it is Vdd +0.3V
According below…
Part Number: TPL0202-10 Hello guys,
One of my customers is considering using TPL0202-10 for their new products.
At this moment, they have the following question about the device. Could you please give me your reply?
Q1. The want to apply 3mV~2200mV to HA…
Part Number: TPL0202-10 hi customer want t o konw 2 questions below;
1) based on datasheet, RTOT value is 8k - 12k, but section 7.4.3 shows the ratio is accurate. if abs value of changed to 8k or 12k, the ratio is also accurate?
2) Layout exampe, do not…
Part Number: TPL0202-10 Hi team,
Do you have any data for long-term drift for TPL0202-10?
I am looking for graph like this (from LT5400).
Best Regards,
Kei Kuwahara
Part Number: TPL0202-10 Hi Team,
The TPL0202-10MRTER has a single rail voltage supply. The customer wants to know if there is a limit on the input voltage of the potentiometer in the negative region. The customer's input voltage has a range of -0.5V to…
Part Number: TPL0202-10 I can not seem to get the TPL0202 to work.
I am designing a amplifier board and using the TPL0202 to set the gain. The processor being used is a PIC (I know I probably should have used a processor from TI).
I read the datasheet…
Other Parts Discussed in Thread: TPL0202-10 Hi team,
Could you tell me what the alternative to the following product ?
・Microchip MCP4362T-503E/ST
Best Regards,
Tomoki
Part Number: TPL0202-10 Dear Expert,
Customer would like to test performance of TPL0202-10.
Because there are no EVM available in TI store, so we want to convert the footprint from QFN to DIP.
Did we have EVM board or footprint converter for TPL0202…
Hi Giovanni,
We have not implemented any impedance control in this design.
The digital potentiometer determine the two thresholds of the two comparators in the board. The value of these two threshold depends on what you are trying to achieve with your…