Part Number: TPL5010 Hi,
Please recommend a watchdog chip.
Temperature -40°C to 125°C
Low power consumption 35nA
Power supply 1.8v-3.3v
Reset pin: Output low
When resetting, a mos tube is needed to power off the mcu
No manual key reset required…
Part Number: TPL5010-Q1 Other Parts Discussed in Thread: TPL5010 Dear TI expert,
Customers use TPL5010-Q1 as the watchdog chip of the MCU, and at the same time connect the RST pin of the MCU to a reset IC, as shown in the figure below, there is currently…
Part Number: TPL5010 Other Parts Discussed in Thread: TPS3852
Can I set something so that I can get the blue color result that I shows in the following picture ?
Is the TPL5010 can meet my requirement ? Or can you suggest another part that can help me…
Part Number: TPL5010-Q1 Hi,
I want to ask a question:
In the TPL5010-Q1 datasheet, the typical value of tRSTn width is defined as 320ms. What is the maximum value?
Because after the completion of VALID_RST, the software needs to give a DONE signal, and…
Part Number: TPL5010-Q1 Hi team,
I have a question regarding TPL5010-Q1.
If I only utilize the timer function of TPL5010-Q1, don't use the watchdog function, what to do with the DONE pin? Will I still need input logic signal to this pin or leave it floated…
Part Number: TPS3813 Other Parts Discussed in Thread: TPL5010 , Hi Experts
My customer want to find a watchdog timer for CPU which operating in 3.3V
I would like to know TPS3813/TPL5010 which one is better or any other choice.
Best
Regards
Brian
Part Number: TPL5010 Other Parts Discussed in Thread: TPL5110 Hi Experts,
Seeking your assistance on this query concerning the TPL5010:
Customers want to use it as a timer for power on delay. So not as usual with a uC. Question is if it is possible to set…
Part Number: TPL5010 I want to use TPL5010 IC in one our company product, which will be subjected to -20 to +80 degC temperature.
The device mentions IC having max Oscillator Accuracy over temperature of +-400 ppm/degC wrt room temperature 25degC.
Lets…