Part Number: TPL5110EVM Hi everyone,
I’m using the TPL5110EVM and for now I’m just testing the accuracy of the component.
I have a problem when I configure a long time for t_ip: the DRV pin jumps to high by itself. In the first figure I have…
Part Number: TPL5110EVM Other Parts Discussed in Thread: TPL5110 Dear all,
As for TPL5110, maximum is 7200 seconds (2 hours).
I would like to use it for longer hours interval such s 5 hourly, 12 hourly and 24 hourly.
May i know if there is any other alternatives…
Part Number: TPL5110EVM Hi,
I have TPL5110EVM (figure attached below).
I having Doubts on pins(J1/J3)&(J2/J4). what is use of these pins.
And then please help me
how to connect external resistor to control timing of DRV pulse ?(Connection )
Part Number: TPL5110EVM Other Parts Discussed in Thread: CC2541 , TPL5100EVM , TPL5110 , CC1310 , CC2650 Hi,
Firstly, i am reading documentation for TPL5110EVM from following link " http://www.ti.com/product/TPL5110/technicaldocuments "
I understand…
Part Number: TPL5110EVM Hi,
I have a doubt on TPL5110EVM
what is the difference between one-shot mode and timer mode in nano timer?
Thanks in Advance
Regards
Ashok
Part Number: TPL5110-Q1 Other Parts Discussed in Thread: TPL5110 , TPL5110EVM Dear
Our company refers to "TPL5110EVM User's Guide" and TPL5110 manual application circuit design One shot mode circuit is as follows:
The test found the following…
Hello Aosker,
Yes, TPL5110 can be used as a 90 minute (4800 second) timer - TPL5110 can delay up to 7200 seconds, or two hours, and offers a one-shot mode. The penultimate entry in datasheet table 3 shows the resistance values that can be used to program…
Dear Douglas
The graph reported in the previous post was made on an TPL5110EVM in timer mode.
We have just replicate the set up you indicated an with a VDD variation a Power On Reset event is triggered.
Only on the rising edge of the VDD triggers the…