Part Number: TPL5111 Other Parts Discussed in Thread: BQ32000 , BQ32002 Dear Team,
Do we have suitable solution can replace BLX8563?
Thanks a lot.
Many Thanks,
Jimmy
Part Number: TPL5111 Other Parts Discussed in Thread: SN74LVC1G125 , SN74LVC1G04 , My use case is this:
EN/ONE_SHOT = GND (one shot mode). TPL5111 M_DRV held high by toggle switch (not momentary) so that DRVn is high all the time (keeps load switch enabled…
Part Number: TPL5111 Hi team,
In the related thread it said that there are is not a PSpice model for the TPL5111, but that was from 5 years ago.
Any chance we now have an unencrypted TPL5111 which customers can use?
Thanks,
Jacob
Part Number: TPL5111 Hello, in the past I tried to use the TPL5111 to turn on the power supply of my circuit. The functionality that I now require is that it resets itself only when it receives a done signal. In other words, I'm looking for a timer that…
Part Number: TPL5111 Other Parts Discussed in Thread: TPL5110 , TPL5010 I have been looking for an IC like the TPL5111 (but opposite sort of) which acts like a timed watchdog to hard reset a MCU. Under normal operation the MCU will 'report in' by pulsing…
Part Number: TPL5111 Hi,
I'm designing a Bluetooth transceiver module that should send a pocket of data for approximately every 30 sec. So I selected a resistance value of 16K for delay.
For testing purpose, I kept the done signal floating and connected…
Part Number: TPL5111 I use a TPL5111 as a timer to power on a uC (after a AP2210/DC-DC) to do some background tasks. The time is set to 1 minute.
A momentary push button (tactile switch) is used to hold M_DRV high for manual power on (to wake up the system…
Part Number: TPL5111 Dear all,
i am designing a low power device and want to use the TPL5111 to trigger the en pin of am LDO.
the Switch is a normal Switch and not a Pushbutton. So it provides a logic high or low the whole time.
The question is what…
Part Number: TPL5111 Hello Team,
I'm posting on behalf of my customer, please see the inquiry below:
I am designing a prototype with the TPL5111 chip but I am getting very unpredictable time between to wake up timing.
I put a resistor of 169k Ohm…
Part Number: TPL5111 Hello I Edwin
I Request TPL5111 DRvN Pin
I want to use the TPL5111 one-shot mode. If DEALY/M_DRV change Status, I want to Stop DRVn.
Is there a way to change it without disconnecting the power? What should I do if I need to shut down…